Skip to main content
p0ulp3
Associate
April 29, 2010
Question

Issues with the independant watchdog

  • April 29, 2010
  • 6 replies
  • 1198 views
Posted on April 29, 2010 at 16:06

Issues with the independant watchdog

    This topic has been closed for replies.

    6 replies

    domen23
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    Huh, dunno, maybe this helps you. I use it to start the watchdog with max timeout (about half a minute at 64 MHz).

    static void watchdog_init()

    {

        if (RCC_GetFlagStatus(RCC_FLAG_IWDGRST))

            printf(''there was a watchdog reset\n'');

        /* lets not ClearFlag, because rtc init does it for us */

        IWDG_WriteAccessCmd(IWDG_WriteAccess_Enable);

        /* 0xfff*256/(30..60)khz -> 17-35s */

        IWDG_SetPrescaler(IWDG_Prescaler_256);

        IWDG_SetReload(0xfff);

        IWDG_ReloadCounter();

        IWDG_Enable();

        /* stop watchdog when core is stopped (debugging) */

        DBGMCU_Config(DBGMCU_IWDG_STOP, ENABLE);

    }

    p0ulp3
    p0ulp3Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    Hi,

    the register CR of DBGMCU is at 0, so the bit DBG_IWDG_STOP is at 0 (0: The watchdog counter clock continues even if the core is halted, based on the datasheet).

    I had also tried to remove the debugger but without any success.

    By looking at the interrupt vector in the datasheet, I can see that there are the Non Maskable Interrupt, the IWDG interrupt, Hardfault Interrupt, and all the maskable interrupts with configurable priorities.

    My question is, if there is a non maskable interrupt, can we say that the IWDG is a maskable interrupt ? and if so, where can I enable this interrupt ?

    Regards

    domen23
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    And what's the value of DBG_IWDG_STOP?

    Alternately, you could just detach the debugger, and see if it works then.
    p0ulp3
    p0ulp3Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    Hi Domen,

    thanks for your reply, basically the example that I use is very similar :

      /* IWDG timeout equal to 280 ms (the timeout may varies due to LSI frequency

     

         dispersion) */

     

      /* Enable write access to IWDG_PR and IWDG_RLR registers */

     

      IWDG_WriteAccessCmd(IWDG_WriteAccess_Enable);

     

     

      /* IWDG counter clock: 40KHz(LSI) / 32 = 1.25 KHz */

     

      IWDG_SetPrescaler(IWDG_Prescaler_32);

     

     

      /* Set counter reload value to 349 */

     

      IWDG_SetReload(349);

     

     

      /* Reload IWDG counter */

     

      IWDG_ReloadCounter();

     

     

      /* Enable IWDG (the LSI oscillator will be enabled by hardware) */

     

      IWDG_Enable();

     

    DBGMCU_Config(DBGMCU_IWDG_STOP, ENABLE);

     

     

      while (1)

     

      {}

     

    Do you had any special configuration to do before launching the IWDG ? some IT to enable for example ?

    Regards

    brianeley9
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    Hi,

    I experienced the exact same symptoms and it turned out that the watchdog could not reset the STM32 because an external power monitor chip was forcing the reset pin high. I disconnected the power monitor chip so that the only thing tied to the micro's reset pin was a 10K pull-up resistor, and the watchdog was suddenly able to reset the processor exactly as expected.

    As a side note, forcing the reset pin high was also preventing software resets from working correctly.

    Hope this saves someone the pain I went through,

    Brian

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    As a side note, forcing the reset pin high was also preventing software resets from working correctly.

     

    Yeah, seen that before, hope you didn't waste too much time. Usually someone driving a -RESET pin with a push-pull driver rather than an open-collector/drain one.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..