Skip to main content
spiovan9
Associate III
June 15, 2010
Question

Int2str function improvement

  • June 15, 2010
  • 7 replies
  • 2561 views
Posted on June 15, 2010 at 17:25

Dear friends,

this improved version of the ''int2str'' function will solve a bug present in the original version provided with the hyperterminal example though it is used nowhere in that example.

I'm working on an application to perform analog conversion and then send the value to the hyperterminal like a simple datalogger. When converting the int data from the adc to a string the original routine doesn't manage the data length changing (i.e. when the data turn from 1024 to 0 the string losses the string termination '\0').

Hope it helps

Stefano

/*******************************************************************************

* Function Name : Int2Str

* Description : Convert an Integer to a string

* Input : - str: The string

* - intnum: The intger to be converted

* Output : None

* Return : None

*******************************************************************************/

void Int2Str(char *str, u32 intnum)

{

u32 Div = 1000000000;

int i, j = 0, Status = 0;

for (i = 0; i < 10; i++)

{

str[j++] = (intnum / Div) + 48;

intnum = intnum % Div;

Div /= 10;

if ((str[j-1] == '0') & (Status == 0))

{

str[j] = '\0';

j = 0;

}

else

{

str[j] = '\0';

Status++;

}

}

}

#string #stm8s-discovery #int2str #int2str
    This topic has been closed for replies.

    7 replies

    Grom
    ST Employee
    July 7, 2010
    Posted on July 07, 2010 at 14:32

    Hello Stefano,

    Thanks for this feedback, I will correct this point in the code sources.

    Rgds

    Grom
    vlad_kn2000
    Associate
    July 9, 2010
    Posted on July 09, 2010 at 06:16

    Workalot
    Associate III
    July 16, 2010
    Posted on July 16, 2010 at 04:16

    Workalot
    Associate III
    July 18, 2010
    Posted on July 19, 2010 at 00:53

    Correction if you please

    -------------------------

    int Int2Str(char *str, u32 intnum)

    { u32 Div = 1000000000L;

      char*  p = str;

    while ( intnum < Div )       // Skip unsignificant zeros

      { Div /= 10;                 //

      }

    while ( Div )        // Convert the number to string {                                         // *p++ = intnum/Div + '0';    // save a digit intnum %= Div;              // Div /= 10;                        // }

    *p    = 0;                    // Append trailing null

      return ( p - str );

               // Return length of string

    }

    -------------------------

    RomainR.
    ST Employee
    July 23, 2010
    Posted on July 23, 2010 at 15:16

    Hi,

    Attached you will found my own string_conversion library. It very usefull when you want use lcd display or uart with terminal interfacing.

    Functions can convert signed/unsigned char, int, double and float into string. And unsigned char into hex and bin format. 

    I hope you enjoy it...

    Zip file (STVD + Raisonance Compiler):

    string_conversion.h

    string_conversion.c

    main.c

    (Note: you should include string.h for strcpy function)

    Regards,

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    spiovan9
    spiovan9Author
    Associate III
    January 23, 2011
    Posted on January 23, 2011 at 19:29

    Hi Romain,

    thankyou very much for the string functions you posted.

    I have just a question: what is the purpose of the SC_BUFFER_OFS_PTR = 5 constant?

    I traced down, for example, the following function ''sc_format'' and found that if you pass to the function u8 digits = 16 (as in a LCD display) or any other value which is > 5, the  *--pstr = SC_FILL_CHAR; goes outside the memory allocation of the buffer string. I.E. it goes under the [0] position of the string buffer.

    Thank you

    Stefano

    /* Function Definition -------------------------------------------------------*/

    // Do formatted output

    u8 *sc_format(u8 *pstr,u8 digits){

     u8 len = (u8)(pstr - SC_BUFFER_OFS_PTR);  // Get length of string

     while (digits--)              // Sting loop

     {

      if (len) // If character created by conversion, just skip left in buffer

      {

       pstr--;

       len--;

      }

      else // It must be a fill character

      {

       *--pstr = SC_FILL_CHAR;

      }

     }

     return pstr;

    }

    RomainR.
    ST Employee
    January 25, 2011
    Posted on January 25, 2011 at 10:34

    Hi Stefano,

    So

    I wrote

    this

    code

    a few years ago

    now

    ,

    I

    'll

    try

    to

    answer

    your questions

    :

    sc_buffer_ofs_ptr is adresse of the string + decimal point number offset.

    u8

    variable

    digit

    in

    all

    functions

    is the

    number of

    characters after

    the

    decimal

    point

    .

    At the

    time

    I

    wanted

    to limit

    that number

    without

    actually

    providing

    security

    easily

    portable

     

    on a

     

    simple

    8-bit

    microcontroller

    .

    It is

    true

    that

    as

    the function

    is written

    ,

    if

    u8

    digit

    >

    5

    it

    goes outside

    of

    the allocation of

    the

    buffer size

    .

    This

    code

    works

    fine,

    but

    it

    is

    not perfect

    .

    I

    suggest you

    limit the

    number

    of

    decimal

    digits

    u8

    = 3. So, 4 work too!

    Regards,

    romain

    From: piovan.stefano

    Posted: Sunday, January 23, 2011 7:29 PM

    Subject: Int2str function improvement

    Hi Romain,

    thankyou very much for the string functions you posted.

    I have just a question: what is the purpose of the SC_BUFFER_OFS_PTR = 5 constant?

    I traced down, for example, the following function ''sc_format'' and found that if you pass to the function u8 digits = 16 (as in a LCD display) or any other value which is > 5, the  *--pstr = SC_FILL_CHAR; goes outside the memory allocation of the buffer string. I.E. it goes under the [0] position of the string buffer.

    Thank you

    Stefano

    /* Function Definition -------------------------------------------------------*/

    // Do formatted output

    u8 *sc_format(u8 *pstr,u8 digits){

     u8 len = (u8)(pstr - SC_BUFFER_OFS_PTR);  // Get length of string

     while (digits--)              // Sting loop

     {

      if (len) // If character created by conversion, just skip left in buffer

      {

       pstr--;

       len--;

      }

      else // It must be a fill character

      {

       *--pstr = SC_FILL_CHAR;

      }

     }

     return pstr;

    }

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.