Skip to main content
prasad2
Associate II
December 22, 2009
Question

stm32f103 DMA receive

  • December 22, 2009
  • 3 replies
  • 1248 views
Posted on December 22, 2009 at 08:00

stm32f103 DMA receive

    This topic has been closed for replies.

    3 replies

    prasad2
    prasad2Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:34

    Hello,

    In STM32 library for DMA related interrupts I can only see following interrupt sources.

    - DMA_IT_TC: Transfer complete interrupt mask

    - DMA_IT_HT: Half transfer interrupt mask

    - DMA_IT_TE: Transfer error interrupt mask

    I have used DMA_IT_TC for UART4 TX to put new data in buffer, how can I use this UART4 Rx? Can I get a interrupt on new data received in buffer by DMA?

    Does any one have a sample program for this?

    Regards,

    Prasad

    jvaque
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:34

    If you know how many bytes you will receive, configure the DMA, and when it receives the specified number of bits, DMA_IT_TC will raise the same way it does for TX.

    (...)

    DMA_InitStructure7.DMA_MemoryBaseAddr = (uint32_t)pBuffer;

    DMA_InitStructure7.DMA_BufferSize = (uint32_t)NumByteToRead;

    (...)

    I2C_DMACmd(I2C1, ENABLE);

    /* Enable the DMA Channel7 Transfer Complete IT */

    DMA_ITConfig(DMA1_Channel7, DMA_IT_TC, ENABLE);

    (...)

    sdodd
    Visitor II
    October 10, 2011
    Posted on October 10, 2011 at 20:45

    I have successufully set up a DMA FIFO in circular mode, to drain the USART when it's RXNE flag is set. I want to change it so that I can do variable len dma's to different buffers. I have implemented this but only the initial DMA cycle fires off.

    I there any reason why I can reprogram the DMA controller and enable the engine within the ISAR? Any examples would be helpful

    Thanks

    Steve