I couldnot make STM32F103RC CANBUS work
hello dear forum,
I copied following code from std peripheral library
however I couldnot make it work
what I am doing wrong ?
thank you
---------------
-
RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);
----------------
NVIC_InitStructure.NVIC_IRQChannel = USB_LP_CAN1_RX0_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 5;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
--------------------------------------
CAN_Initialize(void)
{
CAN_InitTypeDef CAN_InitStructure;
CAN_FilterInitTypeDef CAN_FilterInitStructure;
/* CAN register init */
CAN_DeInit(CAN1);
CAN_StructInit(&CAN_InitStructure);
/* CAN cell init */
CAN_InitStructure.CAN_TTCM=DISABLE;
CAN_InitStructure.CAN_ABOM=DISABLE;
CAN_InitStructure.CAN_AWUM=DISABLE;
CAN_InitStructure.CAN_NART=DISABLE;
CAN_InitStructure.CAN_RFLM=DISABLE;
CAN_InitStructure.CAN_TXFP=DISABLE;
CAN_InitStructure.CAN_Mode=CAN_Mode_LoopBack;
CAN_InitStructure.CAN_SJW=CAN_SJW_1tq;
CAN_InitStructure.CAN_BS1=CAN_BS1_8tq;
CAN_InitStructure.CAN_BS2=CAN_BS2_7tq;
CAN_InitStructure.CAN_Prescaler=1;
CAN_Init(CAN1, &CAN_InitStructure);
/* CAN filter init */
CAN_FilterInitStructure.CAN_FilterNumber=1;
CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdMask;
CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_32bit;
CAN_FilterInitStructure.CAN_FilterIdHigh=0x0000;
CAN_FilterInitStructure.CAN_FilterIdLow=0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdHigh=0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdLow=0x0000;
CAN_FilterInitStructure.CAN_FilterFIFOAssignment=CAN_FIFO0;
CAN_FilterInitStructure.CAN_FilterActivation=ENABLE;
CAN_FilterInit(&CAN_FilterInitStructure);
/* CAN FIFO0 message pending interrupt enable */
CAN_ITConfig(CAN1, CAN_IT_FMP0, ENABLE);
return ;
}
---------------------------
void CAN_TXmit(void){
//
I call this function 10 times every second
CanTxMsg TxMessage;
/* transmit 1 message */
TxMessage.StdId=0x00;
TxMessage.ExtId=0x1234;
TxMessage.IDE=CAN_ID_EXT;
TxMessage.RTR=CAN_RTR_DATA;
TxMessage.DLC=2;
TxMessage.Data[0]=0xDE;
TxMessage.Data[1]=0xCA;
CAN_Transmit(CAN1, &TxMessage);
}
-----------------------
void USB_LP_CAN1_RX0_IRQHandler(void)
{
i++;
this variable never increase - i.e. it never enters interrupt handler
CanRxMsg RxMessage;
CAN_Receive(CAN1, CAN_FIFO0, &RxMessage);
}
#can #stm32f103