Skip to main content
stefanofante9
Associate II
June 9, 2010
Question

STM32F103 USB EXAMPLE

  • June 9, 2010
  • 2 replies
  • 716 views
Posted on June 09, 2010 at 18:20

STM32F103 USB EXAMPLE

    This topic has been closed for replies.

    2 replies

    chikos332
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:54

    Hi,

    are you using the version v3.1.1 of the USB library ? (I think that the isochronous IN is supported only in this version... there was a post about this issue in the past, try to find it).

    Cheers.

    stefanofante9
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:54

    Hi,

    yes I'm using the last version of the libraries 3.1.1

    I'm trying to port an application that I wrote for STR912

    I didn't find any example for an IN transfer using ISOCHRONOUS EP

    I'm able to configure and transfer data using BULK but when I try to select the EP as ISOCHRONOUS no EP irq are generated :( !

    There is a bug in the libs?