Skip to main content
okulicz
Associate II
June 2, 2008
Question

New STM32F103RB module to BUY

  • June 2, 2008
  • 3 replies
  • 984 views
Posted on June 02, 2008 at 08:03

New STM32F103RB module to BUY

    This topic has been closed for replies.

    3 replies

    tta
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:24

    looks really cool :

    http://www.propox.com/products/t_174.html

    only (tiny) issue is we need to make an adapter so our JTAG debuggers can snap in, no direct fit :)

    I also suggest you make a 48 and 100 pin board like this ??

    [ This message was edited by: tta on 25-02-2008 09:52 ]

    okulicz
    okuliczAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:24

    Minimodule with ARM Cortex-3 32-bit microcontroller STMicroelectronics STM32F103RB (128 kB Flash, 20 kB SRAM). Include USB, CAN interface and 8MB SerialFlash.

    0690X00000602gcQAA.jpg

    - Complete, ready to use microprocessor system

    - Fast ARM microcontroller STM32F103Rx with up to 90 DMIPS throughput

    - SerialFlash memory 64Mb (8MB)

    - Reliable reset circuit

    - Built-in system generator 8MHz

    - Built-in 32.768kHz crystal resonator for RTC

    - Built-in voltage regulator 3.3V 400mA

    - Module supply voltage: 3.3V or 3.8 - 16V

    - 2 x 32 terminals with 0.1'' (2.54mm) pitch fitting every prototype board

    - Small dimensions: 40.5mm x 35.5mm

    - Available evaluation board and sample applications

    http://www.propox.com

    [ This message was edited by: okulicz.andrzej on 22-02-2008 09:50 ]

    okulicz
    okuliczAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:24

    I hope, this module interest You:

    0690X00000602ghQAA.jpg

    MMstm32F103VB minimodule

    * Complete, ready to use microprocessor system

    * Fast ARM microcontroller STM32F103Vx with up to 90 DMIPS throughput

    * SerialFlash memory M25P64 64Mb (8MB)

    * Built-In JTAG 20-pin connector (Wiggler compatybile)

    * Reliable reset circuit

    * Built-in system generator 8MHz

    * Built-in 32.768kHz crystal resonator for RTC

    * Built-in voltage regulator 3.3V 400mA

    * Module supply voltage: 3.3V or 3.8 - 16V

    * 2 x 40 terminals with 0.1'' (2.54mm) pitch fitting every prototype board

    * Small dimensions: 61mm x 37.5mm

    * Available evaluation board and sample applications

    http://www.propox.com/products/t_186.html?lang=en

    :o :o :o :o :o :o :o :o