Skip to main content
kang2367
Associate
November 11, 2008
Question

USB Mass storage demo problem

  • November 11, 2008
  • 5 replies
  • 1064 views
Posted on November 11, 2008 at 09:42

USB Mass storage demo problem

    This topic has been closed for replies.

    5 replies

    kang2367
    kang2367Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:51

    Hello everybody.

    I have problem using 'mass storage demo' source.

    I compiled IAR EWARM V5.20.

    Compile and make hex file successfuly. Then download to device.

    But PC can't detect USB device.

    I tested same source with IAR EWARM V5.11.

    Compile & make hex file. Then download to device. It works well.

    Does any additional setting need in compiler version 5.20?

    Or is this problem related to technical note TN0067?

    I used high-density device ST32F103ZE.

    That technical note limited to medium-density device only.

    Thank you.

    jilisegiar
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:51

    can you share the project with EWARM5.20?

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:51

    Hi,

    You are right, TN0067 is applicable only to medium density devices.

    Regards,

    ST1.

    jilisegiar
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:51

    The ST mass storage demo works fine on the STM3210E-Eval board using EWARM5.20. What I suggest: open the working demo (you said that the demo works using EWARM5.11) with EWARM5.20 without doing any modification and see if it will work or not.

    another suggestion try to turn off the optimization.

    kang2367
    kang2367Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:51

    I attached project source with EWARM5.20.

    I modify some part(hw_config.c, platform_config.h) of ST mass storage demo source to match my hardware board.

    It has no compile error. But it does not work.

    I don't know what to do.

    Please help me how to solve this problem.