Question
F4 DMA to SDIO NDTR Problem
Posted on January 26, 2013 at 01:26I have much the same problem as wilczewski.jeffrey. I see it on my F4 Discovery board. If his problem is the same then it�s the DMA2_S3CR_bit.EN = 1; line that makes the problem. I have single stepped through my SD card assembly code and watched NDTR go from 0x0080 to 0xFFFF when setting EN=1.With NDTR set incorrectly the DMA completion interrupt never happens. Always I see 0xFF7F words remaining until DMA completion. At least the data transfer part of DMA works.I�ve tried several ways to set EN=1. All useful ways cause the NDTR change including following the sample F4 Discovery code which uses bit band addressing to set EN=1. (Using the debugger and playing around with the enable flag I was able to set things such that EN=1 and NDTR=0x0080.)I tried the idea from van_hooft.frank.001. Changing the flow controller did not work. FWIW, sample F4 Discovery code sets the peripheral as flow controller. #dma-sdio-ndtr-problem