Skip to main content
ramadevi
Associate II
April 6, 2010
Question

Hardware details required for ADC example

  • April 6, 2010
  • 3 replies
  • 903 views
Posted on April 06, 2010 at 08:59

Hardware details required for ADC example

    This topic has been closed for replies.

    3 replies

    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 13:46

    As already explained to you on the Keil forum, this is clearly shown in the schematics!

    http://www.keil.com/forum/docs/thread16660.asp

    (note that there are additional replies in that thread since your last post there)

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    ramadevi
    ramadeviAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:46

    Dear STM32One,

    Could you please help me?

    ramadevi
    ramadeviAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:46

    I think I failed to explain my doubt.Yes, I have seen the responses at Keil.

    From the schematics, I could understand that the pin PC4 in Extension connector is connected to the on-board pot RV1. I

    I was confused where to connect the variable power supply leads.Because I were able to see values changing for the ADCConvertedValue without connecting variable supply to PC4 and POT not being adjusted.Also when I tested the pins PC4 and GND with a multimeter with POT varying, the voltage goes to 0-3.26V.How then the external supply helps?

    I am novice to this kind of activity and am learning the basics of microcontrollers.