Skip to main content
smart
Associate III
September 4, 2009
Question

can message acceptance filtering

  • September 4, 2009
  • 3 replies
  • 931 views
Posted on September 04, 2009 at 14:44

can message acceptance filtering

    This topic has been closed for replies.

    3 replies

    smart
    smartAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:22

    can anybody help me in setting up the message filtering for CAN

    I want to receive CAN message which are meant for me

    I have running slave devices and I want to get interrupted when I receive the message for that particular ID

    For example In my hardware I read the switch address lets say it is 5.

    Now I want to recive interrupt only when I receive the message the CAN message for node ID 5.

    Can anybody provide me some example code.

    Thanks

    smart
    smartAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:22

    thanks for your reply

    but still my I am not able to receive CAN packet with ID 5

    I been using CAN interrupt and canopen from last one year and I am getting interrupt for every CAN packets but when I use filtering I dont get Interrupts for that particular ID, I dont know whats wrong with the STM32 CAN filtering please help me.

    my code is given below:

    This is the CAN packet that I am sending..

    ID length D0 D1 D2 D3 D4 D5 D6 D7

    0005 8 11 22 44 66 77 88 66 55

    ________________________________________________________________________

    /* CAN filter init */

    CAN_FilterInitStructure.CAN_FilterNumber=0;

    CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdMask;

    CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_32bit;

    CAN_FilterInitStructure.CAN_FilterIdHigh=0x0000; ;

    CAN_FilterInitStructure.CAN_FilterIdLow=0x0005 ; ;

    CAN_FilterInitStructure.CAN_FilterMaskIdHigh=0x0000 ; ;

    CAN_FilterInitStructure.CAN_FilterMaskIdLow=0xFFFF;

    CAN_FilterInitStructure.CAN_FilterFIFOAssignment=CAN_FIFO0 ;

    CAN_FilterInitStructure.CAN_FilterActivation=ENABLE;

    CAN_FilterInit(&CAN_FilterInitStructure);

    /* CAN FIFO0 message pending interrupt enable */

    CAN_ITConfig(CAN1, CAN_IT_FMP0, ENABLE);

    **********CAN interrupt code*****************************

    void USB_LP_CAN1_RX0_IRQHandler(void)

    {

    CanRxMsg RxMessage;

    static Message m = Message_Initializer;

    CAN_Receive(CAN1,CAN_FIFO0, &RxMessage);

    m.cob_id = RxMessage.StdId;

    m.len = RxMessage.DLC;

    m.rtr = 0;

    m.data[0] = RxMessage.Data[0];

    m.data[1] = RxMessage.Data[1];

    m.data[2] = RxMessage.Data[2];

    m.data[3] = RxMessage.Data[3];

    m.data[4] = RxMessage.Data[4];

    m.data[5] = RxMessage.Data[5];

    m.data[6] = RxMessage.Data[6];

    m.data[7] = RxMessage.Data[7];

    ahnniu
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:22

    hi smart.avr,

    The following section of code may be helpful, using older versions of STLIB.

    Code:

    void can_filter_config(void)

    {

    CAN_FilterInitTypeDef CAN_FilterInitStructure;

    /* CAN filter init */

    CAN_FilterInitStructure.CAN_FilterNumber=0;

    CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdMask;

    CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_32bit;

    // Set the node ID that you want to receive

    CAN_FilterInitStructure.CAN_FilterIdHigh=0x0000;

    CAN_FilterInitStructure.CAN_FilterIdLow=0x0005;

    // Mask the high 16 bits,if you don't use the extern mode

    CAN_FilterInitStructure.CAN_FilterMaskIdHigh=0x0000;

    CAN_FilterInitStructure.CAN_FilterMaskIdLow=0xFFFF;

    CAN_FilterInitStructure.CAN_FilterFIFOAssignment=0;

    // enable the filter

    CAN_FilterInitStructure.CAN_FilterActivation=ENABLE;

    CAN_FilterInit(&CAN_FilterInitStructure);

    }

    Good Luck!

    -------------------

    There is a

    http://www.coocox.org/CoOS.htm

    on

    http://www.coocox.org/