Skip to main content
tkjmail2
Associate III
January 5, 2011
Question

Calculation error with long

Posted on January 05, 2011 at 22:35

Calculation error with long

    This topic has been closed for replies.

    6 replies

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:20

    The L suffix means long (32-bit), not long long (64-bit)

    This works in Keil, other combinations result in ''integer operation result is out of range''

                    long long a = (long long)-1154800 * (long long)3289;

    Probably handled by the preprocessor, at the very least it should be folded by the optimizer.

    The LL suffix also works.

                    long a = -1154800 * 3289;

                    long long b = -1154800 * 3289;

                    long long c = -1154800L * 3289L;

                    long long d = (long long)-1154800 * (long long)3289;

                    long long e = -1154800LL * 3289LL;

                    printf(''a %ld\n'',a);

                    printf(''b %lf\n'',(double)b);

                    printf(''c %lf\n'',(double)c);

                    printf(''d %lf\n'',(double)d);

                    printf(''e %lf\n'',(double)e);

    a 496830096                                                                    

    b 496830096.000000                                                             

    c 496830096.000000                                                             

    d -3798137200.000000                                                           

    e -3798137200.000000                                                           

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    tkjmail2
    tkjmail2Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:20

    Hi.

    Now the calculation is correct too, when I just type in numbers. Though Ride7 and the RLINK debugger still shows the decimal representation wrong, as it can't show 64-bit numbers. But if I look in the RAM, the 8MSB's are F's - so the number is: 0xFFFFFFFF1D9D0690, which is correct.

    Though if I just change my calibration matrix variables to long long, the code doesn't work at all, as the calculated x and y is over the screen limit - which shouldn't occour, but it occours on calculation errors.

    The calibration matrix code and more can be seen here: 

    http://pastebin.com/ARy27c5P

    The analog readings go from 0 to 4096. The calibration code works fine on another screen with 320x240 resolution, but on the 800x480 resolution it doesn't work!

    Best Regards

    Thomas Jespersen

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:20

    Appears to function as expected with GNU 4.3.0, both d) and e) create the correct value.

    Using built-in specs.

    Target: arm-eabi

    Configured with: ../gcc-4.3.0/configure --with-pkgversion='WinARM March 2008' --with-bugurl=http://en.mikrocontroller.net/forum/17 --target=arm-eabi --prefix=/c/WinARM --disable-nls --disable-shared --disable-threads --with-gcc --with-gnu-ld --with-gnu-as --enable-languages=c,c++ --enable-interwork --enable-multilib --disable-libssp --disable-libstdcxx-pch --disable-libmudflap --disable-win32-registry --disable-libgomp --with-dwarf2 --program-prefix=arm-eabi- --with-newlib --disable-newlib-supplied-syscalls --disable-libunwind-exceptions --disable-newlib-atexit-dynamic-alloc --with-gmp=/c/winarms/build/gmp_mpfr --with-mpfr=/c/winarms/build/gmp_mpfr -v

    Thread model: single

    gcc version 4.3.0 (WinARM March 2008)

    void write32(long addr, long x)

    {

      *((long *)addr) = x;

    }

    void write64(long addr, long long x)

    {

      *((long long *)addr) = x;

    }

    {

            long a = -1154800 * 3289;

            long long b = -1154800 * 3289;

            long long c = -1154800L * 3289L;

            long long d = (long long)-1154800 * (long long)3289;

            long long e = -1154800LL * 3289LL;

            write32(0x20002000,a);

            write64(0x20002010,b);

            write64(0x20002020,c);

            write64(0x20002030,d);

            write64(0x20002040,e);

    }

    000001E8 A013            add    r0, pc, #76    ; (adr r0, $000238=$1D9D0690)

    000001EA C803            ldmia    r0!, {r0, r1}   ; Load incorrect 64-bit

    000001EC 4B18            ldr    r3, [pc, #96]    ; ($000250=$20002000)

    000001EE 4A19            ldr    r2, [pc, #100]    ; ($000254=$1D9D0690) Load incorrect 32-bit

    000001F0 601A            str    r2, [r3, #0]

    000001F2 3310            adds    r3, #16

    000001F4 E883 0003        stmia.w    r3, {r0, r1}

    000001F8 3310            adds    r3, #16

    000001FA E883 0003        stmia.w    r3, {r0, r1}

    000001FE A010            add    r0, pc, #64    ; (adr r0, $000240=$1D9D0690)

    00000200 C803            ldmia    r0!, {r0, r1}   ; Load correct 64-bit

    00000202 3310            adds    r3, #16

    00000204 E883 0003        stmia.w    r3, {r0, r1}

    00000208 3310            adds    r3, #16

    0000020A E883 0003        stmia.w    r3, {r0, r1}

    00000238 1D9D0690        dd    $1D9D0690       ; 64-bit WRONG

    0000023C 00000000           dd      $00000000

    00000240 1D9D0690        dd    $1D9D0690       ; 64-bit CORRECT

    00000244 FFFFFFFF        dd      $FFFFFFFF

    00000248 2000000A        dd    $2000000A

    0000024C 40011000        dd    $40011000

    00000250 20002000        dd    $20002000

    00000254 1D9D0690        dd    $1D9D0690       ; 32-bit WRONG

    00000258 000AFFFF        dd    $000AFFFF

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    tkjmail2
    tkjmail2Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:20

    Hi Clive.

    I've tried the ''long long'' method, but it didn't work.

    long long e = -1154800LL * 3289LL;

    This still resulted in the 496... number!

    Thomas

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:20

    Ok, your POINT structure should use signed integers (int) as some of your computation generate negative numbers as POINT values are subtracted from each other, and unless casted will be handled as (unsigned int). This was specifically important with the computation of divisor when I tried casting to (double).

    The coefficients seem to be correctly computed.

    In the computation of x and y, you need to use 64-bit temporary results, x and y can remain as 32-bit signed long.

    x = (((long long)matrix.An * xAnalogReading) + ((long long)matrix.Bn * yAnalogReading) + matrix.Cn) / matrix.Divider;

    y = (((long long)matrix.Dn * xAnalogReading) + ((long long)matrix.En * yAnalogReading) + matrix.Fn) / matrix.Divider;

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:20

    Do you have some real world examples for touchptr readings? And some test analogue readings.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..