Skip to main content
cschumann
Associate III
September 30, 2014
Question

STM32L0 RCC_CFGR read-only?

  • September 30, 2014
  • 1 reply
  • 760 views
Posted on September 30, 2014 at 12:11

Hi,

I'm using an STM32L051 microcontroller for a low power application. Actually I am working on a state change between low power and normal operating mode. Therefore I am trying to switch the system clock to PLL but it seems the RCC_CFGR register is read-only for some unknown reasons. I am using the HAL library and the following initialization sequence (directly copied from the examples):

  RCC_ClkInitTypeDef RCC_ClkInitStruct;

  RCC_OscInitTypeDef RCC_OscInitStruct;

  /* Enable Power Control clock */

  __PWR_CLK_ENABLE();

  /* The voltage scaling allows optimizing the power consumption when the device is

     clocked below the maximum system frequency, to update the voltage scaling value

     regarding system frequency refer to product datasheet.  */

  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  /* Enable HSI Oscillator and activate PLL with HSI as source */

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

  RCC_OscInitStruct.HSEState = RCC_HSE_OFF;

  RCC_OscInitStruct.HSIState = RCC_HSI_ON;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

  RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_4;

  RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_2;

  RCC_OscInitStruct.HSICalibrationValue = 0x10;

  if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

    ErrorHandler();

  /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2

     clocks dividers */

  RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);

  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)

    ErrorHandler();

After this sequence the RCC_CFGR:SW bits are switched to HSE (0b11), RCC_CFGR:SWS is HSI (0b01) and RCC_CFGR:PLLSRC is switched to HSE allthough HSE is deactivated and NO external clock source is available. Manual writing to the CFGR register does not change the value.

NOTE: There was no other initialization prior to this sequence.

1. Any ideas what's going wrong?

2. Under which conditions are the RCC registers locked (except the backup domain stuff)?

Thanks in advance,

Carsten Schumann

Prior to this
    This topic has been closed for replies.

    1 reply

    cschumann
    cschumannAuthor
    Associate III
    September 30, 2014
    Posted on September 30, 2014 at 13:05

    Issue is solved and was related to a non-L0 aware debugger in conjunction with changed register addresses from L1->L0.

    @Moderator: Please delete the thread, since the request is invalid.

    Carsten