Skip to main content
dhutchison1945
Associate III
May 24, 2012
Question

stm32l152V8t6 pb4-lcdseg8

  • May 24, 2012
  • 5 replies
  • 1024 views
Posted on May 24, 2012 at 10:56

Hi,

I'm using the emdedded stm32l lcd driver on the stm32L152V8t6 (lqfp 100pin)

 

all segments work well,but on the pb4-lcdseg8 I see a fixed voltage level(about 2.9V)

very near to the vdd voltage.

the lcd glass is ok.

or the stm32l152v8t6 has the pb4-lcdseg8 driver broken or there is an error on the datasheet.

Can someone confirm me that this pin is working as lcd seg driver ?

the following is the port initialization:

/* GPIO PB4 LCDSEG8 */

GPIO_InitStructure.

GPIO_Pin

= GPIO_Pin_4;

GPIO_InitStructure.

GPIO_Mode

=

GPIO_Mode_AF

;

GPIO_Init(GPIOB, &GPIO_InitStructure);

GPIO_PinAFConfig(GPIOB, GPIO_PinSource4,GPIO_AF_LCD) ;

Thanks in advance

    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    May 24, 2012
    Posted on May 24, 2012 at 11:26

    Probably more dependent on the board, on the STM32L152-EVAL it is jumpered either between the JTAG and LDR via JP10

    I'll take a peek at the jumper if I get a chance.

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource4, GPIO_AF_LCD);
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOB, &GPIO_InitStructure);

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    dhutchison1945
    Associate III
    May 24, 2012
    Posted on May 24, 2012 at 11:47

    Good morning Mr. Clive1,

    Thanks in advance for the fast reply.I'm using an empty prototype board without connections on the gpio pins.

    I tried also to configure the port as input pu-pd or output pp-od,I moved the output state high or low, but I always see about 2.9V.

    I will try to use another free segment driver or I will replace the mcu.may be that this port is broken(I agree,strange but possible)

    I don't think that is an issue related to an old library release that I'm using (1.0.0) I hope.

    regards,

    spectre

    Tesla DeLorean
    Guru
    May 24, 2012
    Posted on May 24, 2012 at 12:39

    I don't think that is an issue related to an old library release that I'm using (1.0.0) I hope.

     

    Merging to V1.1.1 wouldn't take much time would it? A quick diff would at least highlight if much had changed

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    dhutchison1945
    Associate III
    May 24, 2012
    Posted on May 24, 2012 at 13:29

    I did a comparison on the gpio.c and on the gpio.h,I don't see differences for the package I'm using.So I'll replace the mcu with a working one.

    regards

    spectre

    dhutchison1945
    Associate III
    June 15, 2012
    Posted on June 15, 2012 at 14:28

    Yes, I confirm you that it was a faulty(damaged) gpio port :)

    regards

    Spectre