Skip to main content
garzarolli
Associate II
March 11, 2010
Question

copy and run a bootloaderfunction to RAM memory

  • March 11, 2010
  • 2 replies
  • 934 views
Posted on March 11, 2010 at 16:55

copy and run a bootloaderfunction to RAM memory

#activation-internal-bootloader
This topic has been closed for replies.

2 replies

Tomas DRESLER
Associate II
May 17, 2011
Posted on May 17, 2011 at 13:43

I guess you needed a little bit different answer:

create such C function in separate file and configure the linker to place the code content of this file into RAM (maybe in RIDE project explorer, maybe by hand-editing the linker file - I don't remember exactly now).

Other compilers use something like __ramfunc or #pragma((__section__ = ''.RAM'')) etc. Please look in the GCC documentation for placing code into RAM, it's there, but well hidden ;)

damh
Associate III
May 17, 2011
Posted on May 17, 2011 at 13:43

I don't know the ride7 toolchain, but the simple internal bootloader can do that.

1) set BOOT0=VCC, BOOT1=GND

2) connect PA9==USART1_TX, PA10==USART1_RX

3) reset the stm32

4) send 0x7F from PC

5) receive ACK from BOOTLOADER

Rest can be read in AN2606.