Skip to main content
thomasblender9
Associate II
May 21, 2010
Question

Adapt USB DFU Bootloader to STM32F103VET6

  • May 21, 2010
  • 3 replies
  • 1037 views
Posted on May 21, 2010 at 13:00

Adapt USB DFU Bootloader to STM32F103VET6

#stm32
    This topic has been closed for replies.

    3 replies

    Nickname12657_O
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:51

    Hi ,

    To tailor USB DFU to your Specific hardware board. in your case it is Primer2 , you have to go to header file : ''platform_config.h'' then Replace these lines :

    #elif defined (USE_STM3210E_EVAL)

    #define USB_DISCONNECT GPIOB

    #define USB_DISCONNECT_PIN GPIO_Pin_14

    #define RCC_APB2Periph_GPIO_DISCONNECT RCC_APB2Periph_GPIOB

    In Primer2,

    http://www.stm32circle.com/resources/download.php?schema_stm32_primer2_1_2.PDF

    , this connection/disconnection is Pin 83 : ''PD3'' , so Try to modify it to :

    #elif defined (USE_STM3210E_EVAL)

    #define USB_DISCONNECT

    GPIOD

    #define USB_DISCONNECT_PIN

    GPIO_Pin_3

    #define RCC_APB2Periph_GPIO_DISCONNECT

    RCC_APB2Periph_GPIOD

    Of course you need to run '' STM3210E_EVAL'' workspace from Ride project.

    Hope it helps you

    0690X0000060MlBQAU.gif

    Cheers,

    STOne-

    thomasblender9
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:51

    Hello,

    I solved the problem. It was a problem of clock configuration.

    I set the USB clock

    RCC_USBCLKConfig(RCC_USBCLKSource_PLLCLK_1Div5);

    so the PLL should be 72MHz. The crystal in PRIMER2 is 12MHz.

    Thank you for your support with the USB Disconnect Pin.

    Best regards

    thomasblender9
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:51

    Hello STOne-32,

    thank you for your answer. I replaced this lines in the header file.

    The result is better than my first try. Now I have a reaction from Windows. Unfortunately I got the message USB-Device not recognized. I installed the DfuSe USB device driver like shown in UM0412. Also the device description couldn't be read, which should be ''STM Device in DFU Mode''.

    Could you help me to solve this problem?

    Best regards

    Thomas