Skip to main content
lowpowermcu
Associate III
June 19, 2014
Question

printf over USB VCP

  • June 19, 2014
  • 1 reply
  • 1138 views
Posted on June 19, 2014 at 13:37

Hi all,

I am trying to retarget printf over USB-VCP and I am stcuk !

I implemented the putc function in the following way:

****************************************

int fputc(int ch, FILE *f)

{

  USBD_CDC_SetTxBuffer(&hUSBDDevice, (uint8_t *)&ch, 1);

  if(USBD_CDC_TransmitPacket(&hUSBDDevice) != USBD_OK)

  {

    /* Device is busy */

    /* what should I return ? */

  }

  return ch;

}

*****************************************

As you know fputc is called by printf for printing a single character and it is called in a loop until all characters are printed.

What I am facing is that it may happen the USB is busy while sending the previous character. What do I have to do at this condition? fputc return -1 ?

PS: I am STM32 Cube V2.0.0 ''18-February-2014''

Thanks

#usb-vcp-printf
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
June 19, 2014
Posted on June 19, 2014 at 16:37

Consider whether you can buffer outgoing characters, send multiple at a time, or wait until a later time if the USB is currently busy.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..