Skip to main content
jjyeh1976
Associate III
September 4, 2009
Question

Math routine with Cosmic free 16k and STVD 4.1.2

  • September 4, 2009
  • 4 replies
  • 969 views
Posted on September 04, 2009 at 07:18

Math routine with Cosmic free 16k and STVD 4.1.2

    This topic has been closed for replies.

    4 replies

    jjyeh1976
    jjyeh1976Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 15:04

    answer my question...

    in the ''Project Settings'' -> Linker -> User Defined options, add

    ''-lm'' will solve this problem.

    but I find another problem, if I declare the v as local variable (in main.c), the returned value never correct, if it is declared as global variable, the returned value is correct, why?

    jjyeh1976
    jjyeh1976Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 15:04

    Hi,

    I need the math function such atan() and acos(), but they seem not return a resonable value, my code

    double v;

    v = atan(0.2);

    v = acos(0.3);

    I observed the ''v'' in debug mode, but not a correct value of atan(0.2) or acos(0.3), what should I do to make these function work?

    Jason

    jjyeh1976
    jjyeh1976Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 15:04

    Hi Luca,

    Thanks for your advisement, I will check for the optimiaztion.

    BTW, the -lm is the linker command that to find the ''libm.xxx'' while

    linking, the xxx is depends on platform. (In linux is .a)

    luca239955_st
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 15:04

    >> if I declare the v as local variable (in main.c), the returned value never correct, if it is declared as global variable, the returned value is correct, why?

    probably an optimization; the result should be correct even with a local variable, but you probably don't see it.

    Regards,

    Luca (Cosmic)

    PS: I don't know what -lm is, but if it works, so be it !