Skip to main content
VK Verma
Associate III
February 25, 2018
Solved

unicleo not working in FFT mode with IKS01A2+ NUCLEO-F401RE with STM32CubeExpansion_MEMS-XT1_V4.2.0

Posted on February 25, 2018 at 09:01

Hi,

unicleo not working in FFT mode with (&sharpIKS01A2+ NUCLEO-F401RE with STM32CubeExpansion_MEMS-XT1_V4.2.0) and its user message window is showing ''AST Protocol: CHK_CheckAndRemove Failed''.

FFT plot is not showing any graph.

0690X00000609ngQAA.png0690X00000609oEQAQ.png

Please help !

Thanks in Advance !!

VK Verma

#x-nucleo-iks01a2 #iks01a2
This topic has been closed for replies.
Miroslav BATEKBest answer
ST Employee
February 26, 2018
Posted on February 26, 2018 at 09:46

I'm not able to replicate the issue.

I see you have Keil uVision program opened, did you modify the FFT_demo example?

Can you please try to use already compiled binary located in binary directory?

5 replies

Miroslav BATEKBest answer
ST Employee
February 26, 2018
Posted on February 26, 2018 at 09:46

I'm not able to replicate the issue.

I see you have Keil uVision program opened, did you modify the FFT_demo example?

Can you please try to use already compiled binary located in binary directory?

VK Verma
VK VermaAuthor
Associate III
February 27, 2018
Posted on February 27, 2018 at 12:02

Hi Miroslav,

your timely response helped us a lot !

I must say that you catch the right point and when I programmed it with binary, it worked 

But now it is not working with Tera-Terminal software at baud rate 115200 bps; 8 data bits; No parity; 1 stop bit; no hard flow control given in the readme.

I will look into this and update you in the post.

Once again, Thank you very much for your support !!

Thanks and Best Regards,

VK Verma

ST Employee
February 27, 2018
Posted on February 27, 2018 at 16:34

Please try 921600 baud.

VK Verma
VK VermaAuthor
Associate III
March 5, 2018
Posted on March 05, 2018 at 09:31

Hi Miroslav,

As per suggestion it is working in 921600 baud rate. Then i think it is wrongly mentioned in ReadMe for 

115200 bps. 

Thanks for your immediate reply !

Please give me one more support (if possible).... can you kindly suggest some documents which will help us to understand FFT library functions given in this file, so that they can be modified and reused in other applications.

Thanks and Best Regards,

VK Verma