Need support for promoting STM32L4 in Capacitive touch sensing applications
- July 2, 2018
- 6 replies
- 4451 views
Posted on July 02, 2018 at 12:49
Hi Friends !
As discussed in my earlier post we have developed 44 Keys capacitive touch key pad with 4 layer PCB board in Matrix touch scheme between two touch TSC groups with Layer 1= top Digital track, Layer 2= shield and touch track, Layer 3= shield and Layer 4 = touch and digital track, based on STM32L452VET6 100 Pin LQFP package using TSC Peripheral and STM touch middle ware.
Although we are using these Touch IPs very frequently and successfully in Non Matrix touch scheme but this is first we have used it in this format to meet the customer requirement for 44 Nos of keys. I have attached Picture of top and bottom of the PCB for your kind reference.
We are facing calibration issues as keys are non sensitive when applied overlay of 1mm of acrylic. We have applied capacitors of upto 68nf but there is no change in the delta and no touch detected.
But without overlay there is the touch detection but poor calibration and response below is the screen shot for the same.
- Screenshot of STM Studio for both cases
When in Ideal State
When a key is pressed without overlay
Kindly advice how to calibrate it by increasing touch sensitivity.
Thanks and Best Regards,
VK Verma
st.mcu
‌
Majerle.Tilen.001