Skip to main content
e_zhui2
Associate
May 4, 2010
Question

How to implement microsecond delay on STM8S103F3?

  • May 4, 2010
  • 4 replies
  • 2462 views
Posted on May 04, 2010 at 03:34

How to implement microsecond delay on STM8S103F3?

    This topic has been closed for replies.

    4 replies

    jeffrey23
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 15:08

    How about the nop instruction approach ?

    ne562
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 15:08

    #define US(us) ( F_CPU / 3000000.0 * us )

    #define MS(ms) US(ms * 1000) // maximum 10ms

    #define _delay( loops ) \

         _asm(''$N: \n decw X \n jrne $L \n nop'', (U16)loops);

    #define _delay_us(us) _delay(US(us))

    void _delay_ms( U16 ms ) {

         while (ms--) {

             _delay_us( 1000 );

         }

    }

    jeffrey23
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 15:08

    Can you explain what the sim()/rim() are in WaitDelay()

    function ?

    My idea is shown as below:

    void I2C_Delay (u8 bTime)

    {

        /*

                                ld  a,(OFST+1,sp)

      72  0007 0a01             dec (OFST+1,sp)

      73  0009 4d               tnz a

      74  000a 26f9             jrne    L13

        */

        bTime /= 3;         // 3.5 cycles each loop !

        while (bTime--)

            ;

    } /* I2C_Delay */

    bTime is in STM8S machine cycles

    (SYSCLK = 1 / 16MHz = 62.5 ns = 0.0625 us) !

    mozra272
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:08

    .ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 p.MsoNormal, .ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 li.MsoNormal, .ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 div.MsoNormal {margin:0in;margin-bottom:.0001pt;font-size:11.0pt;font-family:'Calibri','sans-serif';} .ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 span.EmailStyle15 {font-family:'Calibri','sans-serif';color:windowtext;} .ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 .MsoChpDefault {;} @page Section1 {size:8.5in 11.0in;margin:1.0in 1.0in 1.0in 1.0in;} .ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 div.Section1 {page:Section1;}

    Hi

    Boltnut,

    try this solution:

    /* General Purpose 1µs Time base */

    void Init_TIM2(void)

    {

        /* TimerTick = 1µs

           Warning: fcpu must be equal to 16MHz

           fck_cnt = fck_psc/presc = fcpu/16 = 1MHz --> 1 tick every 1µs

           ==> 1 µs / 1µs = 1 ticks

         */

        TIM2_TimeBaseInit( TIM2_PRESCALER_16, 1);

        TIM2_UpdateRequestConfig(TIM2_UPDATESOURCE_GLOBAL);

        TIM2_ITConfig(TIM2_IT_UPDATE, ENABLE);

        TIM2_Cmd(ENABLE);

    }

    /** Wait a delay

      * @param[in] Delay based on timer Tick

      * @return None

      **/

    void WaitDelay(u16 Delay)

    {

      

    GTimeStamp = 0x00;

        sim();

        while (GTimeStamp <= Delay);

        rim();

    }

    /**

      * @brief Timer2 Update/Overflow/Break Interruption routine.

      * @par Parameters:

      * None

      * @retval

      * None

      */

    #ifdef _COSMIC_

    @far @interrupt void TIM2_UPD_OVF_BRK_IRQHandler(void)

    #else /* _RAISONANCE_ */

    void TIM2_UPD_OVF_BRK_IRQHandler(void) interrupt 13

    #endif /* _COSMIC_ */

    {

        GTimeStamp++;

       

    TIM2_ClearFlag(TIM2_FLAG_UPDATE);

    }

    Regards

    mozra