Skip to main content
Chopra.Deepak
Associate II
February 9, 2018
Question

For confusion on selecting Graphical LCD for STM32F746

  • February 9, 2018
  • 11 replies
  • 2563 views
Posted on February 09, 2018 at 09:42

I would like to develop HMI hardware using STM32F746 with 480x272 Graphical LCd, But i have confusion on selection of Graphical LCD?Am i select Graphical LCD with graphic controller or without graphic controller? STM32F746 inbuilt LCD controller.   

    This topic has been closed for replies.

    11 replies

    T J
    Senior III
    February 9, 2018
    Posted on February 09, 2018 at 10:20

    the easiest way is BuyDisplay 10' Touch RA8876,

    it runs on 2x SPI ports.1 SPI for LCD and 1 SPI for Touch.

    and leaves your processor running full speed without using the on board LCD controller

    https://www.buydisplay.com/default/serial-spi-i2c-10-1-inch-tft-lcd-module-dislay-w-ra8876-optl-touch-panel

     
    Chopra.Deepak
    Associate II
    February 9, 2018
    Posted on February 09, 2018 at 12:32

    Hello TJ,

                          thanks for reply,but i would like to develop a product for home automation system ,so i need many GLCD,and also i have general question,because lcd without graphic controller is cheap.

    T J
    Senior III
    February 10, 2018
    Posted on February 10, 2018 at 01:20

    The alternative is the 4.3' LCD with touch $23 from china

    I paid $35 for an 18' LVDS panel, the drive board I made costs about $15.

    Vitaliy Chernobay
    Senior
    February 12, 2018
    Posted on February 12, 2018 at 19:45

    For 800x600 resolution - only RGB control!

    For example my project 

    https://github.com/golf2109/STM32F746IG-StemWin-800x480

     
    Chopra.Deepak
    Associate II
    February 13, 2018
    Posted on February 13, 2018 at 06:34

    Hello Vitaliy,

                             Yes,i knowi,STM32F7xx able to control RGB,but i would like to know GLCD used by you is with inbuilt GLCD Controller or you use STM32F7xx as GLCD Controller? 

    Vitaliy Chernobay
    Senior
    February 13, 2018
    Posted on February 13, 2018 at 20:39

    I used STM32F769 for control GLCD with RGB interface.

    I tried control GLSD 800x480 with  SSD1963 controller.

    It is very very slow to fill screen1-2 sec for 800x480.

    My project for SSD1963

    https://github.com/golf2109/STM32F429ZI_SSD1963_FT5336

     
    AVI-crak
    Senior
    February 13, 2018
    Posted on February 13, 2018 at 21:37

    ER-TFT070-4 800 * 480, one contact 3.3V power supply digital part. RGB 8 * 8 * 8. 18 dollars.

    The minimum headache when connecting to the st chip, without additional intermediate interfaces.

    A large resolution weakly improves image quality, but very well increases the price. On sale there are RGB displays without a built-in D / A converter and a high-voltage stabilizer - from $ 4. Such cheap displays can be used in the presence of experience in analog circuitry.