Skip to main content
apullin
Associate III
March 16, 2018
Question

Selecting pins for I2C1 and I2C2, if AF4 covers ''I2C1...3'' ?

  • March 16, 2018
  • 5 replies
  • 3259 views
Posted on March 16, 2018 at 16:56

Hi folks,

I am a little confused by the AF selection on some pins in the case of using multiple I2C's.

I am bringing up a new board where board I2C1 and I2C2 are being used on an F4 micro.

I2C1 is on PB6 & PB7, I2C2 is on PB9 & PB10.

Looking at the MCU manual, it shows for the GPIO AF multiplexer: 'AF4 (I2C1..3, I2CFMP1)'

If I set PB9 to AF4, how is there a distinction between the pin functioning for I2C1 or I2C2?

#i2c #gpio #f4
This topic has been closed for replies.

5 replies

waclawek.jan
Super User
March 16, 2018
Posted on March 16, 2018 at 23:40

0690X0000060A9MQAU.png
apullin
apullinAuthor
Associate III
March 17, 2018
Posted on March 17, 2018 at 06:23

Thanks for the diagram. I don't think this exactly captured the point I was confused about, but nearly: if there was a wire from the I2C2_SDA node up to AF9 of PB9, that would reveal what I was missing.

waclawek.jan
Super User
March 17, 2018
Posted on March 17, 2018 at 10:02

if there was a wire from the I2C2_SDA node up to AF9 of PB9, that would reveal what I was missing.

Should you tell us the particular mcu model you had on your mind, I would have probably guessed what's the source of your confusion and I'd put that wire there.

'an F4 micro' for me is 'F405/'F407/'F415/'F17, as those were the first in the line, historically, and I am working with them a lot.

The crystal ball has its limitations, at least the cheapo model I am using  ;)

JW

Tesla DeLorean
Guru
March 17, 2018
Posted on March 17, 2018 at 03:00

The pin routing on individual pins is clearly shown in the Data Sheet tables. AF Mux on the pin is a 16-to-1 routing, I2C1 presumably has NO routing to PB9, where AF4 is connected to an I2C2 SDA node internally.

Each pin has its own MUX, each mux connects to different NODES.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
apullin
apullinAuthor
Associate III
March 17, 2018
Posted on March 17, 2018 at 06:20

 ,

 ,

Aha.

 ,

So my confusion was partly from using an old version of the ST libraries, which ,has a section of the gpio header with:

♯ define

GPIO_AF_I2C1

((

uint8_t

)

0x04

)

/* I2C1 Alternate Function mapping */

♯ define

GPIO_AF_I2C2

((

uint8_t

)

0x04

)

/* I2C2 Alternate Function mapping */

♯ define

GPIO_AF_I2C3

((

uint8_t

)

0x04

)

/* I2C3 Alternate Function mapping */

That confused me, so looking at the manual, I saw that indeed AF4 was allocated for I2C1..3. But what I missed was that AF9 is also a candidate for I2C1..3 connections.

Now that I look into the actual pin function matrix in the device datasheet per your recommendation, I do see that for PB9, AF4 = I2C1_SDA, but AF9 = I2C2_SDA , for PB9.

 ,

Which led me to check further in st32f4xx_gpio.h, and sure enough, it has:

♯ define

GPIO_AF9_I2C2

((

uint8_t

)

0x09

)

/* I2C2 Alternate Function mapping (Only for STM32F401xx/STM32F410xx/STM32F411xE/STM32F412xG/STM32F413_423xx Devices) */

♯ define

GPIO_AF9_I2C3

((

uint8_t

)

0x09

)

/* I2C3 Alternate Function mapping (Only for STM32F401xx/STM32F411xE/STM32F412xG and STM32F413_423xx Devices) */

So I just had to be cognizant of heterogenous ,mappings for the pin muxes, and make the right choices for my project using the old ST libraries.

 ,

Generating a minimum working example using CubeMX, it does correctly select the pin-specific AF value:

GPIO_InitStruct.

Alternate

=

GPIO_AF9_I2C2,

I swear, 'It was right there in the damn datasheet' is going to be the quote on my tombstone ... ,