Skip to main content
mehmet.karakaya
Associate III
July 11, 2017
Question

how to install st-link/v2 driver in win10 ?

  • July 11, 2017
  • 20 replies
  • 8403 views
Posted on July 11, 2017 at 18:24

hello dear forum,

I bought a win10 laptop

where I tried to connect st-link/v2 adaptor

I downloaded stsw-link009 package and tried to install 

however I get the message 

'you have to run 64bit version of DPInst.exe on this computer'

I couldnot find this version in internet

how to proceed ?

please advice

thank you

#st-link #win10
This topic has been closed for replies.

20 replies

Zt Liu
Senior III
July 12, 2017

Posted on July 12, 2017 at 09:20

 

mehmet.karakaya
Associate III
July 12, 2017
Posted on July 12, 2017 at 19:37

hello Zhitai, 

I saw it too, however... 

isn't it for AMD processors ?

mehmet.karakaya
Associate III
July 13, 2017
Posted on July 13, 2017 at 10:31

hello 

please advice

ST Technical Moderator
July 13, 2017
Posted on July 13, 2017 at 12:02

Hello,

You should launch 

stlink_winusb_install.bat  file that will determine the .exe to be run.

Otherwise, the installation of ST-Link Utility will install the driver automatically by the installshield.

With Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
mehmet.karakaya
Associate III
July 13, 2017
Posted on July 13, 2017 at 12:56

hello thank you,

I did run '

stlink_winusb_install.bat' (even with admin rigths) in cmd window

still the message 

'you have to run 64bit version of DPInst.exe on this computer'

I mean dont anybody use st-link with win10 ?

how did they do the installation ?

ST Technical Moderator
July 13, 2017
Posted on July 13, 2017 at 16:02

Hi

karakaya.mehmet

Please confirm which version are you using?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
mehmet.karakaya
Associate III
July 13, 2017
Posted on July 13, 2017 at 16:25

I use Windows 10 with INTEL i5 processor

I have ST-LINK / V2

I try to install stsw-link009 package

mehmet.karakaya
Associate III
July 14, 2017
Posted on July 14, 2017 at 10:46

still unanswered

please advice

MARK Sylvia888
Visitor II
July 14, 2017
Posted on July 14, 2017 at 11:03

I have the same question�?thanks guys!

Vangelis Fortounas
Associate II
July 14, 2017
Posted on July 14, 2017 at 12:50

Hello !  Try to change the path of installing directory by make a new folder e.g at root directory ->  c:\abc. Put inside the uncompressed driver  and run it again.

mehmet.karakaya
Associate III
July 14, 2017
Posted on July 14, 2017 at 13:40

I have added screenshot

0690X00000603tdQAA.jpg
Vangelis Fortounas
Associate II
July 14, 2017
Posted on July 14, 2017 at 13:51

This message is not from bat file.  Is from dpinst_x86.exe.   Try to run  directly with administrator rights the dpinst_amd64.exe 

Vangelis Fortounas
Associate II
July 14, 2017
Posted on July 14, 2017 at 14:00

At least try this.

 Go to Control Panel and open Device Manager.

 Find the stlink device(or the unknown usb device)

Right click the device and select properties.

Select Driver tab, then click the Update Driver button.

Choose Browse my computer for driver software.

Let me pick from a list of device drivers on my computer

 Browse for the .inf driver file in your unziped stlink folder. Open and Next.

The driver must be installed.

mehmet.karakaya
Associate III
July 14, 2017
Posted on July 14, 2017 at 15:51

thank you Vangelis, it worked

why there is no readme file in the package ?

It took 3 day of me :(

Oscar Lopez
Visitor II
March 21, 2018
Posted on March 21, 2018 at 19:05

Hi

I?ve tried to follow all the considerations mentioned and still have the same error on my Windows10

a) downloaded

http://www.st.com/en/development-tools/stsw-link009.html

 

b) unzip and run as with administrator privileges the bat file

0690X00000604UxQAI.jpg

c) review Device Manager under unknown usb device and try to upgrade indicating to the .inf folder, it fails with '' Device Description Request Failed''

Any ideas?

Thanks for answering 

Oscar

Oscar Lopez
Visitor II
March 23, 2018
Posted on March 23, 2018 at 09:31

Thank you all, for sharing the previous posts

Solved!!

In my case it was an inference with the Antivirus Software (corporative) and I had to disable it (surprinsingly , not the rest of the guys of my team making the same instalation, behavoural protection? )

After failed running the .bat file stlink_winusb_install.bat, finally I got it, running directly 'dpinst_amd64'

Cheers

Oscar