Associate III
December 28, 2012
Question
why winsock cannot get my UDP packet ?
- December 28, 2012
- 5 replies
- 1876 views
Posted on December 28, 2012 at 15:01
#udp-winsock
#include ''stm32f4xx_conf.h''
#include ''ethernet.h''
#include <stdio.h>
#include <string.h>
//source IP
#define S_IP1 192
#define S_IP2 168
#define S_IP3 1
#define S_IP4 100
//dest IP
#define D_IP1 192
#define D_IP2 168
#define D_IP3 1
#define D_IP4 2
struct
ip_eth_addr {
uint8_t addr[4];
};
struct
mac_addr {
uint8_t addr[6];
};
struct
ip_eth_addr s_ip = { {S_IP1, S_IP2, S_IP3, S_IP4}};
struct
ip_eth_addr d_ip = { {D_IP1, D_IP2, D_IP3, D_IP4}};
struct
mac_addr mymac = { {0x1c, 0x9a, 0x65, 0x4a, 0xd9, 0x6c} } ;
struct
mac_addr destmac = { {0xff, 0xff, 0xff, 0xff, 0xff, 0xff} } ;
char
ipstring [20];
void
* first_data_byte;
//define ethernet II header
struct
eth_header
{
//ether frame
uint8_t ether_dest[6];
//destination mac address
uint8_t ether_src[6];
//source mac address
uint16_t ether_type;
//ether type
//ip frame
uint8_t vhl;
//version / IHL
uint8_t tos;
//type of service
uint16_t len;
//len
uint16_t ipid;
uint16_t ipoffset;
uint8_t ttl;
uint8_t proto;
uint16_t ipchksum;
uint16_t srcipaddr[2];
//26
uint16_t destipaddr[2];
//udp
uint16_t srcport;
uint16_t destport;
uint16_t udplen;
uint16_t udpchksum;
};
//struct eth_header frame;
#define frame ((struct eth_header*)&uip_buf[0])
unsigned
char
frame_counter;
unsigned
int
test_counter;
char
test1[] =
''TEST''
;
unsigned
int
data_len = 64;
//udp data len
void
send_UDP_frame(
void
)
{
frame_counter++;
uip_len =
sizeof
(
struct
eth_header);
//get struct header len = 42
memcpy
(frame->ether_dest, &destmac, 6);
//0xff = broadcast
memcpy
(frame->ether_src, &mymac, 6);
frame->ether_type = HTONS(0x0800);
//IP following
frame->vhl = 0x45;
//IP4, 20byte header
frame->tos = 0x00;
//
frame->len = HTONS(28 + data_len);
frame->ipid = HTONS(frame_counter);
//
frame->ipoffset = HTONS(0);
frame->ttl = 0x80;
//time to live
frame->proto = 0x11;
//UDP (17)
frame->ipchksum = 0;
//reset checksum (will be calculated and inserted later)
memcpy
(frame->srcipaddr, &s_ip,4);
//insert source ip
memcpy
(frame->destipaddr,&d_ip,4);
//insert dest ip
//calculate IP4 header checksum
frame->ipchksum=~uip_chksum((uint16_t*)&uip_buf[14],20);
//20 byte header checksum
frame->srcport = HTONS(1024);
//source port
frame->destport = HTONS(1023);
//destination port
frame->udplen = HTONS(data_len+8);
//data len + 8 byte udp header
tapdev_send(uip_buf,uip_len+data_len);
}
hello forum,
I am trying to send an empty UDP packet to visual basic 6.0 winsock
as you can see in attached picture wireshark ''sees'' theUDP packets
howeverwinsock never go into below subroutine ( it doesnot getthe packets)
what is the missing thinghere?
thank you
Private
Sub
Winsock1_DataArrival(
ByVal
bytesTotal
As
Long
)
Text1 = bytesTotal
Dim
strData
As
String
Winsock1.GetData strData, vbString
End
Sub
#udp-winsock