Skip to main content
mehmet.karakaya
Associate III
May 15, 2017
Question

which usart is used for bootloader in F103RC ?

  • May 15, 2017
  • 1 reply
  • 516 views
Posted on May 15, 2017 at 16:19

Hello dear forum,

In my F103RC project I need to connect USART inputs RX2 and RX1 to each other

( I have my PCB produced already, thats why )

I want use flash loader demo with USART1 

my question ;

which usart is used other than USART1 during bootloader function

does RX2 have a function during bootload ? - ( I want it to be floating input without a function during bootload )

is this possible ?

thank you 

#stm32f103-bootloader
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
May 15, 2017
Posted on May 15, 2017 at 16:30

Try reading App Note AN2606?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..