Question
STM32F4 FMC on non-multiplexed SRAM
Posted on June 30, 2016 at 11:55
Hi,
I plan to build a board with an STM32F446VE + IS66WV51216EBLLAs the STM32F446VE is a 100pin package, it does not offer non-multiplexed interface on the FMC.So I was considering using the FMC in multiplexed PSRAM mode, and adding a latch like the 74LVC373AD device (to transform the multiplexed interface to non-multiplexed interface), but it seems that the FMC_NL ( = NADV ) line is inverted ..Couldn't find if it was possible to invert FMC_NL logic, so I suppose I can't.Consequently, it seems I should add an inverter before the latch.Sounds tricky in the end, and as I couldn't find any example on the internet of someone using the multiplexed FMC on non-multiplexed PSRAM, I wonder is this can really work ..Any advice ?Thanks and best regards,Vincent. #stm32f4 #sram #- #fmc