Skip to main content
gdiez
Associate III
September 15, 2010
Question

Problems with the ADC TIME CONVERSION

  • September 15, 2010
  • 5 replies
  • 1119 views
Posted on September 15, 2010 at 09:14

Problems with the ADC TIME CONVERSION

    This topic has been closed for replies.

    5 replies

    gdiez
    gdiezAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:07

    The CODE is...

    STM32f10xx_it.c

    void TIM1_UP_IRQHandler(void)

    {

    GPIOA->BSRR = GPIO_Pin_4; /* Toggle PIN */

    TIM1_ClearITPendingBit(TIM1_FLAG_Update); /* Clear UPDATE interrupt bit */

    }

    void ADC_IRQHandler(void)

    {

    GPIOA->BRR = GPIO_Pin_4; /* Toggle PIN */

    ADC1->SR = ~((u16)0x0004); /* Clear ADC interrupt bit */

    }

    I code the main features like that.

    main.c

    ---------------------------------------------------------------------------------

    ---------------------------------------------------------------------------------

    NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4); /* Sin Group Priority, PRI-n[7:4] Subpriority */

    NVIC_SETPRIMASK(); /* DESHABILITA las interrupciones para configuracion */

    /* Configure and enable ADC interrupt */

    NVIC_InitStructure.NVIC_IRQChannel =

    ADC1_2_IRQChannel;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStructure);

    NVIC_InitStructure.NVIC_IRQChannel =

    TIM1_UP_IRQChannel; /* TIM1 Update Interrupt */

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; /* Valor de prioridad [0~15] */

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; /* Valor de subprioridad */

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; /* Habilita la interupción elegida */

    NVIC_Init(&NVIC_InitStructure);

    NVIC_RESETPRIMASK(); /* HABILITA las interrupciones despues de configuracion */

    ---------------------------------------------------------------------------------

    ---------------------------------------------------------------------------------

    RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_7); /* SYSCLK=56MHZ*/

    RCC_ADCCLKConfig(RCC_PCLK2_Div4); /* ADC PCLK2/4=14MHz - CONFIGURE RCC_CFGR.ADCPRE */

    RCC_PCLK2Config(RCC_HCLK_Div1); /* APB2 PCLK2 = 56MHz */

    RCC_HCLKConfig(RCC_SYSCLK_Div1); /* AHB HCLK = 56MHz CONFIGURE RCC_CFGR.HPRE */

    ---------------------------------------------------------------------------------

    ---------------------------------------------------------------------------------

    ADC_InjectedChannelConfig(ADC1, ADC_Channel_15, 1, ADC_SampleTime_1Cycles5);

    gdiez
    gdiezAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:07

    Anyone knows the answer?

    Can it be the time lost going to the ISR?

    I´ve somo doubts with the TIM1 overflow interrupt, because i have to enable it only to see the exact time that ADC starts, not to work the ADC, only to know this time.

    May i doing it bad?

    lowpowermcu
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:07

    Hi Gerardo,

    Why you don't use systick timer. I think it is useful for time measurement and perhaps it is more accurate than using GPIO.

    Herzlich,

    MCU Lüfter

    gdiez
    gdiezAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:07

    Hi lowpower:

    I tried what you say but i couldn´t achive any thing.

    I configure the systick with 3us time, to ensure that it nevers downflows.MI strategie is turn ON the systick system when the TIM1 overflows (like i did with toggle pin, but with systick timer).

    when the ADC finishes, I enter in its ISR, and then I turn OFF the systick timer. Then with a breakpoint and a debugger, I saw the register STK_VAL(Value of systick).

    I thought that this time of systick must be 1us but, when I enable the systick, my code never leaves the TIM ISR. If I delete the code it alternates TIM and ADC ISR.

    I´m getting a little bit confused.

    My configuration is the following:

    void TIM1_UP_IRQHandler(void)

    {

      SysTick_CounterCmd(SysTick_Counter_Enable); 

      TIM1->SR &= ~ 1;                               /* Clears TIM1 FLAG */

    }

    void ADC_IRQHandler(void)

    {     

          SysTick_CounterCmd(SysTick_Counter_Disable);

          SysTick_CounterCmd(SysTick_Counter_Clear);

          ADC1->SR = ~((u16)0x0004);                               /* Clears ADC FLAG */

    }

    Main.c

    SysTick_SetReload(168);   /* A frecuencia de 56MHz 3uS */

    gdiez
    gdiezAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:07

    I´ve tried it to see it in oscilloscope. I will investigate your way to do it and I will tell you if I get a solution.

    Thks for replying!!