Skip to main content
nanayakkaraan
Associate III
May 6, 2011
Question

STM32 I2C communication failure

  • May 6, 2011
  • 5 replies
  • 798 views
Posted on May 06, 2011 at 13:16

STM32 I2C communication failure

    This topic has been closed for replies.

    5 replies

    greg_t
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:34

    Post your code

    ColdWeather
    Senior
    May 17, 2011
    Posted on May 17, 2011 at 14:34

    You can take a look at

    http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/stm32_i2c_cpal.zip

    library available on ST website.

    In general, I2C peripheral in STM32F is tricky and not really successful: well minded double buffering of data register brings in fact a lot of problems, the cases for one or two bytes transmissions should be handled in a special way while the interrupts should be completely disabled, etc. I spent a week to get familiar with STM32F I2C. Be ready!
    emalund
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:34

    read the errata, there is a lot of problems with the I²C but two workarounds are suggested

    lowpowermcu
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:34

    I have found a library for I2C that I find useful to handle I2C communicatio without requiring to understand the I2C spec.

    I want to share it with you and hope it helps you:

    http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/stm32_i2c_cpal.zip

    lowpowermcu

    emalund
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:34

    read the errate. two workarounds suggested

    0x00000040, as the return value of I2C_GetLastEvent(). same as me (and probably everybody else)