Skip to main content
philipweiss
Associate II
October 31, 2017
Solved

st25r3911b transparent mode example

  • October 31, 2017
  • 2 replies
  • 1255 views
Posted on October 31, 2017 at 19:51

Is there any sample code to put the ST25R3911B into transparent mode?  I have been unable to make the 

ST25R3911B output OOK in transparent mode.

I need this functionality because I'm implementing a proprietary protocol.

My configuration/use model:

  • My circuit uses MCU_CLK as required for timing

  • I configure the ST25R3911_REG_OP_CONTROL register to enable TX and disable RX

  • I clear ST25R3911_REG_AUX_tr_am and set ST25R3911_REG_AUX_ook_hr in the ST25R3911_REG_AUX register to enable OOK.
  • I execute the 0xDC command (ST25R3911_CMD_TRANSPARENT_MODE) to enable transparent mode.
  • I configure the MOSI pin to push-pull output 
  • I expect changes to MOSI to be reflected when I measure from RFO1 to RFO2, with an oscillating signal (MOSI high), or nothing (MOSI low).

But, unfortunately, I don't get any signal on RFO1/RFO2.

Any assistance would be greatly appreciated.

    This topic has been closed for replies.
    Best answer by Ulysses HERNIOSUS

    Posted on December 14, 2017 at 15:28

    Hello,

    unfortunately ST does not have support code showing usage of transparent mode on ST25R3911B.

    Looking through your procedure looks reasonable. Some paths to look into:

    • You don't mention oscillator enabling 'en' bit: I assume you did that. Not getting any signal might sound like this.
    • ook_hr should not be needed, I am not exactly aware what happens if ==1
    • Please observe that /SS line is not going low again after the Enter Tansparent Mode command.

    Regards, Ulysses

    2 replies

    Ulysses HERNIOSUS
    ST Technical Moderator
    December 14, 2017

    Posted on December 14, 2017 at 15:28

    Hello,

    unfortunately ST does not have support code showing usage of transparent mode on ST25R3911B.

    Looking through your procedure looks reasonable. Some paths to look into:

    • You don't mention oscillator enabling 'en' bit: I assume you did that. Not getting any signal might sound like this.
    • ook_hr should not be needed, I am not exactly aware what happens if ==1
    • Please observe that /SS line is not going low again after the Enter Tansparent Mode command.

    Regards, Ulysses

    philipweiss
    Associate II
    December 19, 2017
    Posted on December 19, 2017 at 01:35

    I'm sorry to hear that ST does not have any support for transparent mode.  I have been, however, able to make some changes to the code to make both transmit and receive work in transparent mode.

    Thanks for your help.