Skip to main content
harinath
Associate III
August 6, 2013
Question

STM32W108xx IRQC configuration

  • August 6, 2013
  • 3 replies
  • 617 views
Posted on August 06, 2013 at 19:20

Hello all,

I'm working on STM32W108xx & interfacing a sensor whose interrupt pin connected to the PB7, IRQC pin. How to configure this pin for the following handler ?

void
EXTIC_IRQHandler(
void
)
{
if
(EXTI_GetITStatus(EXTI_IRQC))
{
EXTI_ClearITPendingBit(EXTI_IRQC);
}
}

I tried to call simply the following function, but doesn't work.

NVIC_EnableIRQ(EXTIC_IRQn);

It looks that this Interrupt configuration is bit different from the STM32 based MCUs. Any code sample would be a great help. #stm32w108
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    August 6, 2013
    Posted on August 06, 2013 at 19:51

    void STM_EVAL_PBInit(Button_TypeDef Button, ButtonMode_TypeDef Button_Mode)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    EXTI_InitTypeDef EXTI_InitStructure;
    NVIC_InitTypeDef NVIC_InitStructure;
    /* Configure Button pin as input */
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_PUD;
    GPIO_InitStructure.GPIO_Pin = BUTTON_PIN[Button];
    GPIO_Init(BUTTON_PORT[Button], &GPIO_InitStructure);
    /* Set pull-up on button I/O */
    GPIO_SetBits(BUTTON_PORT[Button], BUTTON_PIN[Button]);
    if (Button_Mode == BUTTON_MODE_EXTI)
    {
    /* Configure Button EXTI line */
    EXTI_InitStructure.EXTI_Source = BUTTON_EXTI_SOURCE[Button];
    EXTI_InitStructure.EXTI_IRQn = BUTTON_EXTI_IRQn[Button];
    EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling_Edge;
    EXTI_InitStructure.EXTI_LineCmd = ENABLE;
    EXTI_InitStructure.EXTI_DigitalFilterCmd = ENABLE;
    EXTI_Init(&EXTI_InitStructure);
    /* Enable and set Button EXTI Interrupt to the lowest priority */
    NVIC_InitStructure.NVIC_IRQChannel = BUTTON_IRQn[Button];
    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F;
    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F;
    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
    NVIC_Init(&NVIC_InitStructure);
    }
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    August 6, 2013
    Posted on August 06, 2013 at 19:57

    {
    GPIO_InitTypeDef GPIO_InitStructure;
    EXTI_InitTypeDef EXTI_InitStructure;
    NVIC_InitTypeDef NVIC_InitStructure;
    // PB7, check also other clocks, GPIO, SYSCLK or whatever
    /* Configure Button pin as input */
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_PUD;
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;
    GPIO_Init(GPIOB, &GPIO_InitStructure);
    /* Set pull-up on button I/O */
    GPIO_SetBits(GPIOB, GPIO_Pin_7);
    /* Configure Button EXTI line */
    EXTI_InitStructure.EXTI_Source = EXTI_SourcePB7;
    EXTI_InitStructure.EXTI_IRQn = EXTI_IRQC;
    EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling_Edge;
    EXTI_InitStructure.EXTI_LineCmd = ENABLE;
    EXTI_InitStructure.EXTI_DigitalFilterCmd = ENABLE;
    EXTI_Init(&EXTI_InitStructure);
    /* Enable and set Button EXTI Interrupt to the lowest priority */
    NVIC_InitStructure.NVIC_IRQChannel = EXTIC_IRQn;
    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F;
    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F;
    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
    NVIC_Init(&NVIC_InitStructure);
    }
    void EXTIC_IRQHandler(void)
    {
    if(EXTI_GetITStatus(EXTI_IRQC) == SET)
    {
    EXTI_ClearITPendingBit(EXTI_IRQC);
    // Do something
    }
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    harinath
    harinathAuthor
    Associate III
    August 10, 2013
    Posted on August 10, 2013 at 03:54

    Works perfect. Thank you clive1.