Skip to main content
christos
Associate II
July 2, 2015
Question

SPI connect to SPWF01SC

  • July 2, 2015
  • 3 replies
  • 801 views
Posted on July 02, 2015 at 16:04

Hi,

I'd like to use the SPI connection of SPWF01SC.

Could you say me please which pinout description are right?

Is the the DocID025635 Rev 2 and the STEVAL-IDW001V1 with SPI description right?

http://www.mikrocontroller.net/attachment/229286/spwf01.pdf

Or the DocID025531 Rev 5 without SPI?

http://www.st.com/web/catalog/sense_power/FM2185/SC1930/PF258592

Thanks
    This topic has been closed for replies.

    3 replies

    Gerardo GALLUCCI
    ST Employee
    July 2, 2015
    Posted on July 02, 2015 at 16:10

    Hi Chris,

    there is no SPI interface on SPWF module

    Gerardo GALLUCCI
    ST Employee
    July 2, 2015
    Posted on July 02, 2015 at 16:32

    SPI, I2C, etc, are peripherals from internal STM32.

    They are exported on module's GPIOs, but cannot be used with a standard firmware.

    Standart FW only allows AT-commands through UART. I'm sorry for misunderstanding.