Skip to main content
Mich1
Associate III
December 7, 2017
Solved

STM32 lowest current?

  • December 7, 2017
  • 9 replies
  • 1620 views
Posted on December 07, 2017 at 16:00

Which STM32 has the actual lowest running current consumption (active from flash)?

#stm32-lowest-current
    This topic has been closed for replies.
    Best answer by Andrew Neil
    Posted on December 07, 2017 at 16:57

    http://www.st.com/en/development-tools/st-mcu-finder.html

     

    http://www.st.com/content/st_com/en/product-selector.html

     - indeed there is a column for mA/MHz !

    9 replies

    Andrew Neil
    Super User
    December 7, 2017
    Posted on December 07, 2017 at 16:12

    define, 'running' ?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Mich1
    Mich1Author
    Associate III
    December 7, 2017
    Posted on December 07, 2017 at 16:18

    called 'run mode' in ST datasheet

    Andrew Neil
    Super User
    December 7, 2017
    Posted on December 07, 2017 at 16:32

    Well, you can get mA/MHz figures for the core from the datasheets - but the actual running current of the entire chip will depend on what peripherals you use, and how you use them ...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Mich1
    Mich1Author
    Associate III
    December 7, 2017
    Posted on December 07, 2017 at 16:49

    I hoped ST could advise a component for a new design but it is true that I can read all STM32 datasheets.

    Andrew Neil
    Super User
    December 7, 2017
    Posted on December 07, 2017 at 16:54

    I guess they should be able to tell you the lowest mA/MHz number - but, as noted, there's a lot more to it than just that!

    Have you spoken to you local FAE and/or Distributor?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Mich1
    Mich1Author
    Associate III
    December 7, 2017
    Posted on December 07, 2017 at 17:08

    Unfortunatly, only LDO mode is indicated.

    From the STM32L476: 100 μA/MHz run mode (LDO Mode)  39 μA/MHz run mode (@3.3 V SMPS Mode)

    But is a good start, thanks a lot.

    Szymon PANECKI
    Senior III
    December 11, 2017
    Posted on December 11, 2017 at 09:04

    Hello,

    Regarding STM32 MCUs, which consume the smallest current consumption in RUN mode, I would like to highlight two families:

    http://www.st.com/en/microcontrollers/stm32l0-series.html?querycriteria=productId=SS1817

    based on Cortex-M0+ and

    http://www.st.com/en/microcontrollers/stm32l4-series.html?querycriteria=productId=SS1580

    based on Cortex-M4F. These two families are defenitely the best in whole STM32 portfolio in terms of current consumption (including RUN mode).

    In both families I would propose to focus on devices, which have small amout of resources, especially memory (Flash, SRAM), as this factor has impact on current consumption. In STM32L0 family such devices are

    http://www.st.com/content/ccc/resource/technical/document/datasheet/42/c0/ab/e5/71/7a/47/0b/DM00206508.pdf/files/DM00206508.pdf/jcr:content/translations/en.DM00206508.pdf

    . Theys can consume the current down to 76 uA/MHz in RUN mode. In STM32L4 family by using the same approach we should select

    http://www.st.com/content/ccc/resource/technical/document/datasheet/group3/83/b3/60/f6/b1/cc/47/7e/DM00257211/files/DM00257211.pdf/jcr:content/translations/en.DM00257211.pdf

    . Here the smallest expected consumption is 84 uA/MHz in RUN mode.

    Additionally some of STM32L4 MCUs support a SMPS, which allows to bypass the embedded LDO and reduce the consumption even more. For example

    http://www.st.com/content/ccc/resource/technical/document/datasheet/f7/a0/fc/27/24/4e/4f/3f/DM00257192.pdf/files/DM00257192.pdf/jcr:content/translations/en.DM00257192.pdf

    , with SMPS, will consume only 36 uA/MHz in RUN mode.

    Regards

    Szymon