STM32479I-EVAL Camara to USB Aplication
- 14 replies
- 2892 views
Hi,
I recently bought the STM32479I-Eval board and now I'm testing the sample applications included in STM32Cube_FW_F4_V1.14.0
The application 'STM32469I_EVAL\Applications\Camera\Camera_To_USBDisk' does not work as expected, the LCD screen shows the messages:
USB Init...
Camera Init...
and then:
Press TAMPER button to take a snapshot
Camera Play
but only a fully blank image on the LCD. When I press the tamper button to save the image:
Camera stopped...
Picture Prepared...
Saving Picture in File image_x.bmp...
Header BMP written...
BMP data Pixed save ongoing...
the LED1 is on to indicate the end of saving operation and a message is displayed:
File image_x.bmp saved in USB Disk...
but the image that is saved (Attach file) is completely blank.
Should I need to modify the position of some other* jumper or even modify the code of the example to run this application in STM32479I-Eval?
* Note:
JP3 of STM32479I-EVAL board is on position PC0.
USB key into the STM32479I-EVAL board through 'USB micro A-Male to A-Female' cable (connector CN8).
Thanks in advance,
Sergio
#stm32479i-eval #stm32469i-eval #camera #stm32f479xx