Skip to main content
Martin.Sergio
Associate III
October 5, 2017
Solved

How to Add A Linked File Resource in System Workbench for STM32?

  • October 5, 2017
  • 4 replies
  • 5838 views
Posted on October 05, 2017 at 08:25

Hi,

I´m using a STM32F469I_Eval and in the Examples provides with STM32Cube_FW_F4, I can see that there are some Linked Resources (FILES). If I edit the .project file there are something like that:

<link>

<name>Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal.c</name>

<type>1</type>

<locationURI> copy_PARENT1/Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal.c</locationURI>

</link>

<link>

<name>Drivers/BSP/STM32469I_EVAL/stm32469i_eval.c</name>

<type>1</type>

<locationURI>copy_PARENT1/Drivers/BSP/STM32469I_EVAL/stm32469i_eval.c</locationURI>

</link>

But if I want to create my own project I only can create a Linked Resource (FOLDER). If I edit the .project there are something like that:

<link>

<name>HAL</name>

<type>2</type>

<location>C:/workspace/SystemWorkbenchForSTM32/STM32F4xx_HAL_Driver</location>

</link>

<link>

<name>STM3246I_EVAL</name>

<type>2</type>

<location>C:/workspace/SystemWorkbenchForSTM32/STM32469I_EVAL</location>

</link>

How can I link a File Resource like does ST? (without editing the .project file) I can´t find this option in eclipse menus

Thanks in advance,

Sergio

    This topic has been closed for replies.
    Best answer by Vangelis Fortounas
    Posted on October 05, 2017 at 21:15

    Hello Sergio!

    You can add a Linked File Resource as below.

    Right click to folder that you want to add the file  ->New->File.

    Click 'Advanced' button.

    Check  'Link to File in the File System'  checkbox.

    Click button 'browse'

    And choose the file you want.

    Regards

    vf

    4 replies

    Martin.Sergio
    Associate III
    October 5, 2017
    Posted on October 05, 2017 at 11:23

    I asked in System Workbench for STM32 Forum also

    http://www.openstm32.org/forumthread5855

     

    Still No Answer...

    Vangelis Fortounas
    Associate II
    October 5, 2017
    Posted on October 05, 2017 at 21:15

    Hello Sergio!

    You can add a Linked File Resource as below.

    Right click to folder that you want to add the file  ->New->File.

    Click 'Advanced' button.

    Check  'Link to File in the File System'  checkbox.

    Click button 'browse'

    And choose the file you want.

    Regards

    vf

    Martin.Sergio
    Associate III
    October 13, 2017
    Posted on October 13, 2017 at 09:27

    Hello,

      

    Is it possible to add more than one file at a time?

    Regards

       Sergio

    Vangelis Fortounas
    Associate II
    October 13, 2017
    Posted on October 13, 2017 at 23:00

    Hello,

    I don't know a way to choose many files and to  add at a time.

    But by adding a folder, same way as file , adds also all the contents of the folder.

    Regards.

    vf