Skip to main content
andrewberlin9
Associate
August 3, 2011
Question

stack use monitor

  • August 3, 2011
  • 4 replies
  • 2210 views
Posted on August 03, 2011 at 15:06

I'd like to add stack usage monitoring to my application. I can't afford the overhead of stack checking on every function call, so I was considering adding a routine that runs periodically to monitor the stack high-water mark. I'm not using an RTOS.

I know my stack size, but how do I find the beginning of the stack? will it always start at the same place? I'm using the Keil tools, if that makes a difference.

Thanks!
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    August 3, 2011
    Posted on August 03, 2011 at 17:41

    The stack is set by the first vector on the STM32, and descends from there. The C startup code may also place it too, before calling main().

    A 4K stack, on a 20K part, can nominally get placed at 0x20005000 and descend to 0x20004000. Fill that space with a distinctive pattern, and enumerate upward to measure the depth used.

    In Keil the bottom of the stack is defined by Stack_Mem, and the top/start as __initial_sp

    My stack checker loads a pointer to Stack_Mem, and the climbs 32-bits at a time until if find the bottom of the used stack, and then computes the amount used based on the known size.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    andrewberlin9
    Associate
    August 3, 2011
    Posted on August 03, 2011 at 21:04

    Thank you; conceptually I understand what to do, but I'm getting stuck on the implementation, perhaps because I'm new to the Keil/ARM tools. Now that you've steered me towards the appropriate linker symbols, I can't seem to reference them (__initial_sp and Stack_Mem) from my C code; the linker complains the symbols are undefined. I tried declaring them as extern but it didn't help.

    Tesla DeLorean
    Guru
    August 3, 2011
    Posted on August 04, 2011 at 01:05

    In stm32F10x.s (startup.s, whatever)

                    EXPORT Stack_Size

                    EXPORT Stack_Mem

    Stack_Size      EQU     0x00001000

                    AREA    STACK, NOINIT, READWRITE, ALIGN=3

    Stack_Mem       SPACE   Stack_Size

    __initial_sp

    in C application

    extern void * Stack_Mem;

        unsigned long *p = (unsigned long *)&Stack_Mem;

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    andrewberlin9
    Associate
    August 4, 2011
    Posted on August 04, 2011 at 17:18

    I was missing the EXPORT statements; it works now.

    Thanks!