Skip to main content
tre2020067
Associate III
September 11, 2011
Question

help understanding simple timer and led blink app

  • September 11, 2011
  • 3 replies
  • 1003 views
Posted on September 11, 2011 at 05:01

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    3 replies

    munk2k
    Associate
    September 11, 2011
    Posted on September 11, 2011 at 11:52

    1. how is the timer configured to work with specific pins.

    Its not as such, its just configure to run ''void Timer1IntrHandler (void)'' every-time its event is triggered, you will need to look into the function called within this function to see what its doing to the LED's

    2. how does this app keep looping if there is a empty while(1) at the end?

    It will keep looping within the while(1) forever but when the timer event is triggered it will ''jump'' out of the loop to execute the code from within the time handler function then once finished it will jump back into the while.

    3. why does only PE.6 flash and PE.5 solid?

    Again look inside the function being called by the timer function

    4.how does the timer cause an interrupt?

     

    Erm...its an interrupt timer?? don't really know how to explain this one simpler..

    Perhaps you should play around with Systick first as its much easier to understand.

    Darren.

    tre2020067
    Associate III
    September 11, 2011
    Posted on September 12, 2011 at 01:04

    thanks!!!

    Andrew Neil
    Super User
    September 12, 2011
    Posted on September 12, 2011 at 08:28

    ''how does this app keep looping if there is a empty while(1) at the end?''

    This is fundamental to the concept of interrupts in any processor (not just STM32):

    An interrupt, as the name suggests, interrupts the current flow of execution to execute its ''handler'' or ''service routine'' (aka ''Interrupt Service Routine'', or ''ISR'' for short).

    Once the ISR is complete, normal execution resumes from the point at which it was interrupted...

    In your case, ''the current flow of execution'' is the empty 'while' loop.

    http://en.wikipedia.org/wiki/Interrupt

    http://en.wikipedia.org/wiki/Interrupt_handler

    Keil has a useful booklist here:

    http://www.keil.com/books

     - they aren't (all) specific to Keil...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.