Skip to main content
milan23
Associate
March 13, 2018
Question

Measuremet of internal temperature on ST32F303RCT6

  • March 13, 2018
  • 6 replies
  • 1744 views
Posted on March 13, 2018 at 18:46

We have been using processor temperature measurement for a long time with different families of STM32: M3, F3, F4. Only the processor STM32F303RCT6 does not work. The measured voltage of the sensor is 2.22V and is relatively unstable (voltage for 25C is 1.43V). I just created a simple project that only measures the internal temperature sensor. This program works on STM32F303VCT6 but does not work on STM32F303RCT6. The conditions are exactly the same, 8MHz oscillator, 3.3V power supply. Other measurements in full application work normally. It seems like the internal temperature sensor is not connected to the internal input 16 of the ADC1 converter. Does anyone have a similar experience?

    This topic has been closed for replies.

    6 replies

    waclawek.jan
    Super User
    March 13, 2018
    Posted on March 13, 2018 at 18:52

    Do you use the appropriate sampling time; AVDD/AVSS connected correctly and decoupled; etc.?

    This program works on STM32F303VCT6 but does not work on STM32F303RCT6.

    What is the value of  DBGMCU_IDCODE (at 0xE004 2000) for both?

    JW

    milan23
    milan23Author
    Associate
    March 14, 2018
    Posted on March 14, 2018 at 15:25

    STM32F303RCT6: 0xE0042000: 0x10036422

    STM32F303VCT6: 0xE0042000: 0x10036422

    I found another problem. On RCT6 is not working also Vrefint measurement on ADC1. ADC value is 4095 on ADC_Channel_Vrefint. On ADC2 Vrefint measurement is OK.

    Best Regards,

    Milan

    ________________

    Attachments :

    image001.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxrB&d=%2Fa%2F0X0000000b1v%2FD3kZpw3.JhRRY4f8pOuY8vSnn15DuakS3rH0SKaQWeQ&asPdf=false
    waclawek.jan
    Super User
    March 14, 2018
    Posted on March 14, 2018 at 23:12

    Except of what I've written above, I am out of ideas, sorry.

    JW