Question
Are Pull-ups needed for SDIO
Posted on September 23, 2011 at 03:30
Hello,
I noticed that the schematic for the STM3220G-EVAL which uses an STM32F207 has a 47K pull-up on each of the non-power pins associated with the micro-sd card. I am currently designing a very space constrained board so I would like to avoid any extra components. Are these resistors needed for SDIO communication with an SD card to work? Can internal pull-up resistors be used? I wasn't able to find much information on this, so any insight would be helpful. #stm32-sdio