Skip to main content
csuson
Associate
September 25, 2011
Question

Accessing iNEMO from an embedded linux device

  • September 25, 2011
  • 6 replies
  • 1306 views
Posted on September 25, 2011 at 18:13

has anybody tried accessing the iNEMO board from an embedded linux device using the usb interface? I am able to power the iNEMO from my device and also able to load a usb-serial driver. What I don't know is the correct serial interface parameters to use to open the port. I hope that somebody in this forum has already gone through this exercise.

thx!

#inemo
    This topic has been closed for replies.

    6 replies

    Fabio
    Associate II
    September 28, 2011
    Posted on September 28, 2011 at 14:09

    You can find useful information in the ''UM1017: STEVAL- MKI062V2 communication protocol'' available at ww.st.com/inemo.

    Regards

    Fabio

    csuson
    csusonAuthor
    Associate
    September 28, 2011
    Posted on September 28, 2011 at 22:35

    Hi Fabio,

    I've read that document which is very helpful but I could not find any mention of serial parameters i need to use to open the port like (baud rate, data bits, stop bit, parity and flow control) settings.

    regards.

    Fabio
    Associate II
    September 30, 2011
    Posted on September 30, 2011 at 15:46

    There are no favorite settings for the virtual com over the usb (if you want you can set the bps 115200 and 8N1 with no control flow: hothese values are not used)

    Best Regards

    iNEMO Team

    hg_it
    Visitor II
    October 4, 2011
    Posted on October 05, 2011 at 01:57

    The following code works for me:

    ========

        int     fd;

        struct  termios inemo;

        if((fd = open(port, O_NOCTTY|O_RDWR)) < 0){

            perror(''open'');

            _exit(errno);

        }

        tcgetattr(fd, &inemo);

        inemo.c_iflag &= ~(IGNBRK | BRKINT | PARMRK | ISTRIP | INLCR | IGNCR | ICRNL | IXON);

        inemo.c_oflag &= ~OPOST;

        inemo.c_lflag &= ~(ECHO | ECHONL | ICANON | ISIG | IEXTEN);

        inemo.c_cflag &= ~(CSIZE | PARENB);

        inemo.c_cflag |= CS8;

        tcsetattr(fd, TCSANOW, &inemo);

    =======
    csuson
    csusonAuthor
    Associate
    October 5, 2011
    Posted on October 05, 2011 at 06:15

    I was able to access the inemo board now. It turned out that I need to modify my usb2serial driver. Thx for the help anyways.

    gianluca23
    Visitor II
    September 27, 2012
    Posted on September 27, 2012 at 23:14

    Hi there,

    I have the same problem. I'm not able to talk with the device. Coul'd you please more detailed on ''modify my usbtoserial'' driver ?

    Thanks in advance.