Skip to main content
fiim
Associate III
July 22, 2013
Question

Switch between Mass Storage and Custom HID in Composite project

  • July 22, 2013
  • 2 replies
  • 829 views
Posted on July 22, 2013 at 09:36

Hellow! (stm32f37)�?�ow would you organize Switch between Mass Storage and Custom HID in Composite project? Where is the variable, changing which can be initialized either hid or mass storage or together?

    This topic has been closed for replies.

    2 replies

    dthedens23
    Associate
    July 22, 2013
    Posted on July 22, 2013 at 17:14

    The USB Host (PC) enumerates the device. It does this by asking questions that the device must respond to. The configuration is constant so these answers are coded in structures in flash. This happens when the device is inserted.

    Single Device can be a MS or

    Single Device can be HID or

    Composite Device can be both MS and HID by using more endpoints

    Single Device cannot switch enumeration on the fly (without some special considerations)

    there are examples of composite devices.

    attached custom HID + CDC

    ________________

    Attachments :

    CDC_HID_Composit.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0db&d=%2Fa%2F0X0000000bc2%2FSelgCS.nW7ArpMI8nlxDyZ1GmUCeKbL73.sZHfM8Fjs&asPdf=false
    fiim
    fiimAuthor
    Associate III
    July 22, 2013
    Posted on July 22, 2013 at 21:49

    Thank you! So, if I want to switch between the 3 types, I should have in my program(flash) 3 patterns: Composite_DeviceDescriptor[], HID_DeviceDescriptor[] and MassStorage_DeviceDescriptor[]. Now I have to uninitialize (USB_deinit) the previous and re-initialize using a different descriptor. So?