Skip to main content
zabel
Associate III
November 22, 2017
Question

STM32F756 Ethernet needs DTCM

  • November 22, 2017
  • 3 replies
  • 1060 views
Posted on November 22, 2017 at 12:57

Hi,

I have problems with ethernet (using the HAL library 1.8.0) on the STM32F756ZG.

If I place the DMA buffers in the DTCM (0x20000000-0x2000ffff), it works fine. If I place the DMA buffer anywhere else (SRAM1, SRAM2), I get only on every second ping an answer (50% loss).

I don't use the MPU and I don't activate the data cache (SCB.CCR.DC = 0).

I also tried (despite the dcache being deactivated) flushing the data cache (SCB_DCacheClean()) before sending data in low_level_output() and invalidating the data cache (SCB_DCacheInvalidate()) before reading data in low_level_input(), but to no avail.

Does anybody has an idea?

TIA,

  diz

    This topic has been closed for replies.

    3 replies

    zabel
    zabelAuthor
    Associate III
    November 22, 2017
    Posted on November 22, 2017 at 13:01

    Oops, misspelled the cache control calls, meant SCB_InvalideatDCache() and SCB_CleanDCache().

    zabel
    zabelAuthor
    Associate III
    November 30, 2017
    Posted on November 30, 2017 at 10:23

    Really no one has an idea? Will move on to STM32F765 due to other reason anyway -- will be interesting to see if the same occurs on this MCU.

    zabel
    zabelAuthor
    Associate III
    December 4, 2017
    Posted on December 04, 2017 at 16:22

    My problem was solved by

    https://community.st.com/0D50X00009XkgffSAB

    , i.e. I added __DSB() to HAL_ETH_TransmitFrame() as suggested by daniel nielsson.

    After changing to STM32F765 that fix no longer seems to be necessary.

    STM32F765 is r1p0, STM32F756 is r0p1