Skip to main content
markhaslehurst
Associate
February 23, 2011
Question

STM32 discovery board serial (RS232) communication

  • February 23, 2011
  • 2 replies
  • 950 views
Posted on February 23, 2011 at 18:01

I have just got one of these boards, but as a noob, I am really struggling to get the USART working. I want to display information on the computer. I understand that the ST_LINK cannot do UART over the built in USB cable (ITM Debug). Is this correct?

So.. I have been looking at pins PA9 and PA10, but cannot see anything coming out. I have the following code. Could someone please take a look and see if they can see my problem?? I have spent hours on this! Thanks all!

code:

&sharpinclude ''stm32F10x.h''

&sharpinclude ''STM32vldiscovery.h''

&sharpinclude ''stm32f10x_usart.h''

&sharpinclude ''stm32f10x_rcc.h''

&sharpinclude <stdio.h>

&sharpdefine  LSE_FAIL_FLAG  0x80

&sharpdefine  LSE_PASS_FLAG  0x100

void Delay(uint32_t nTime);

int main(void)

{

 initAll();

 while(1)

 {

 }

}

void initGPIO (void)

{

  /* Enable GPIOx Clock */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);

 

  /* Initialise LEDs LD3&LD4, both off */

  STM32vldiscovery_LEDInit(LED3);

  STM32vldiscovery_LEDInit(LED4);

 

  STM32vldiscovery_LEDOff(LED3);

  STM32vldiscovery_LEDOff(LED4);

 

  /* Initialise USER Button */

  STM32vldiscovery_PBInit(BUTTON_USER, BUTTON_MODE_EXTI);

}

void initSysTick (void)

{

 /* Setup SysTick Timer for 1 msec interrupts  */

 if (SysTick_Config(SystemCoreClock / 1000))

 {

  /* Capture error */

  while (1);

 }

}

void initLSE (void)

{

 /* Enable access to the backup register => LSE can be enabled */

 PWR_BackupAccessCmd(ENABLE);

 

 /* Enable LSE (Low Speed External Oscillation) */

 RCC_LSEConfig(RCC_LSE_ON);

 

 /* Check the LSE Status */

 while(1)

 {

  if(LSE_Delay < LSE_FAIL_FLAG)

  {

   /* check whether LSE is ready, with 4 seconds timeout */

   Delay (500);

   LSE_Delay += 0x10;

   if(RCC_GetFlagStatus(RCC_FLAG_LSERDY) != RESET)

   {

    /* Set flag: LSE PASS */

    LSE_Delay |= LSE_PASS_FLAG;

    /* Turn Off Led4 */

    STM32vldiscovery_LEDOff(LED4);

    /* Disable LSE */

    RCC_LSEConfig(RCC_LSE_OFF);

    break;

   }       

  }

  else /*if(LSE_Delay >= LSE_FAIL_FLAG)*/ /* LSE_FAIL_FLAG = 0x80 */ 

  {         

   if(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET)

   {

    /* Set flag: LSE FAIL */

    LSE_Delay |= LSE_FAIL_FLAG;

    /* Turn On Led4 */

    STM32vldiscovery_LEDOn(LED4);

   }       

   /* Disable LSE */

   RCC_LSEConfig(RCC_LSE_OFF);

   break;

  }

 }

}

void initUART (void)

{

 GPIO_InitTypeDef GPIO_InitStructureTx;

 GPIO_InitTypeDef GPIO_InitStructureRx;

 USART_InitTypeDef USART_InitStructure;

 RCC_APB1PeriphClockCmd(RCC_APB2Periph_USART1 | RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE);  // Enable clocks

 GPIO_InitStructureTx.GPIO_Pin = GPIO_Pin_9;                // Configure TX pin

 GPIO_InitStructureTx.GPIO_Mode = GPIO_Mode_AF_PP;              // Push-Pull

 GPIO_InitStructureTx.GPIO_Speed = GPIO_Speed_2MHz;              // 50MHz

 GPIO_Init(GPIOA, &GPIO_InitStructureTx);                // Initialise

 GPIO_InitStructureRx.GPIO_Pin = GPIO_Pin_10;               // Configure RX pin

 GPIO_InitStructureRx.GPIO_Mode = GPIO_Mode_IN_FLOATING;             // Push-Pull

 GPIO_InitStructureRx.GPIO_Speed = GPIO_Speed_2MHz;              // 50MHz

 GPIO_Init(GPIOA, &GPIO_InitStructureRx);                // Iniitialise

 USART_InitStructure.USART_BaudRate = 57600;                // Set USART1 Baud Rate

    USART_InitStructure.USART_WordLength = USART_WordLength_8b;            // Set USART1 Word Length

    USART_InitStructure.USART_StopBits = USART_StopBits_1;             // Configure USART1 Stop Bits

    USART_InitStructure.USART_Parity = USART_Parity_No;              // Configure USART1 Parity Bits

    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;       // Configure USART1 Flow Control

    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;           // Set USART1 Operation Mode

 USART_Init(USART1, &USART_InitStructure);                // Configure UART

 USART_Cmd(USART1, ENABLE);                    // Enable UART

 //setvbuf(stdout, NULL, _IONBF, 0);

    //printf(''USART1 Inisialised\n'');

 USART_SendData(USART1, 'c');

 //while (!(USART1->SR & USART_FLAG_TXE));

    //USART1->DR = (0x35);

}

void initAll (void)

{

 initGPIO();

 initSysTick();

 initLSE();

 initUART();

}

There is also a file which provides the delay procedure, using the SysTick.

Thanks for any help or guidance!

#stm32 #discovery #usart #rs232
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
February 24, 2011
Posted on February 24, 2011 at 01:28

RCC_APB1PeriphClockCmd(RCC_APB2Periph_USART1 | RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE);  // Enable clocks

 

RCC_APB2PeriphClockCmd(); Perhaps?
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
markhaslehurst
Associate
February 24, 2011
Posted on February 24, 2011 at 10:14

Hi. Thanks for your reply! That seems to have helped a lot!

Now that I look closer at the arguments being passed, that does seem to make sense!