Skip to main content
apavone9
Associate II
October 18, 2016
Question

STM32 ERRI Error Interrupt

  • October 18, 2016
  • 1 reply
  • 734 views
Posted on October 18, 2016 at 16:47

Hi,

In some condition ERRI Interrupt occours without any other error condition (CAN_ESR = 0). What is the meaning of this interrupt?

Thank you.

Alessandro
    This topic has been closed for replies.

    1 reply

    slimen
    Visitor II
    October 28, 2016
    Posted on October 28, 2016 at 16:59

    Hello,

    - ERRI: Error interruptThis bit is set by hardware when a bit of the CAN_ESR has been set on error detection andthe corresponding interrupt in the CAN_IER is enabled. Setting this bit generates a statuschange interrupt if the ERRIE bit in the CAN_IER register is set.This bit is cleared by software.

    - ERRIE: Error interrupt enable

      0: No interrupt will be generated when an error condition is pending in the CAN_ESR.

     1: An interrupt will be generation when an error condition is pending in the CAN_ESR.

    You have to refer to the reference manual for more details on this topic.

    Regards