Skip to main content
Asantos
Associate III
November 6, 2017
Question

NUCLEO-H743ZI LWIP using STM32cubeMX?

  • November 6, 2017
  • 4 replies
  • 867 views
Posted on November 06, 2017 at 11:11

Hi, 

 I generated a simple LWIP/UDP project for the NUCLEO-H743ZI using the STM32cubeMX. But the function HAL_ETH_Transmit(&heth, &TxConfig, 0); returns with DMA error . 

 My board works using the example from the STM32Cube_FW_H7_V1.1.0. So the hardware is ok. 

 What is wrong with my configuration?

 Ari.

    This topic has been closed for replies.

    4 replies

    Amel NASRI
    ST Technical Moderator
    November 6, 2017
    Posted on November 06, 2017 at 11:58

    Hi

    Mendes.Ari

    ‌,

    Before analyzing deeply the problem you are reporting, could you please check from your side that problems reported in

    https://community.st.com/0D50X00009XkYPnSAN

    are fixed at your side, or may be you aren't in the same conditions.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Jeanne Joly
    Associate
    February 15, 2018
    Posted on February 15, 2018 at 17:54

    Hi

    Mendes.Ari

    ,

    Please have a look to the new comments in the following thread

    https://community.st.com/0D50X00009XkYPnSAN

    .

    I hope it will help you.

    BR. Jeanne

    Asantos
    AsantosAuthor
    Associate III
    February 15, 2018
    Posted on February 15, 2018 at 20:28

    Jeanne,

    My problem was that the STM32CubeMx generates a LwIP project using the DTCM RAM (0x20000000). I had to modify the linker file to point to the AXI SRAM (0x24000000) instead.

    There's a way to modify the memory region in the STM32CubeMx project configuration? I think that the default should be AXI SRAM for the H7.

       Ari.

    March 15, 2018
    Posted on March 15, 2018 at 15:28

    I agree you with the suggestion to set the default memory region to AXI SRAM on H7 or to make it as configuration in CubeMX. I've searched many hours to find the issue for my SPI+DMA problem.

    https://community.st.com/0D50X00009XkX4ZSAV