Skip to main content
Uwe Bonnes
Chief
February 28, 2018
Question

STM32F76 datasheet and maximum voltage during programming

  • February 28, 2018
  • 4 replies
  • 732 views
Posted on February 28, 2018 at 12:16

Hello,

ds11532 rev 6 on page 153 in table 57 talks about a maximum supply voltage of 3.0 volt with 32-bit flash program operation. This number seems inconsistant with a maximum voltage of 3.6 for 8 and 16 bit flash programming. The F74x datasheet also has 3.0 Volt as maximum for 32-bit programming?

This topic has been closed for replies.

4 replies

Uwe Bonnes
Chief
March 5, 2018
Posted on March 05, 2018 at 12:34

Can anybody care for this question?

Andrew Neil
Super User
March 5, 2018
Posted on March 05, 2018 at 13:14

Note that this is essentially  a user-to-user forum.

If you want direct ST support, you will need to contact ST direct - possibly via your distributor.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Uwe Bonnes
Chief
March 5, 2018
Posted on March 05, 2018 at 14:37

Andrew, did you really have a look at the datasheet problem I report? Are obvious datasheet error really things that should get reported to the FAEs?

Amel NASRI
ST Technical Moderator
March 5, 2018
Posted on March 05, 2018 at 15:28

Hi

Bonnes.Uwe

‌,

You are right: 3V is wrong as maximum programming voltage with 32-bit program, it has to be replaced by 3.6 as we can see in the relevant reference manual:

0690X00000609tAQAQ.png

This is reported to be fixed in STM32F7 datasheets. Thanks for highlighting.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.