Skip to main content
Uwe Bonnes
Chief
June 18, 2018
Question

ADC2_DMA_RMP[1] on STM32F334 (Rm0364)

  • June 18, 2018
  • 1 reply
  • 461 views
Posted on June 18, 2018 at 11:04

Hello,

as there is no DMA2 on the STM32F334, the SYSCFG->CFGR3 Bit 9 ADC2_DMA_RMP[1] has a misleading description. Following the description, is has to be kept set. 10.1.8 SYSCFG configuration register 3 (SYSCFG_CFGR3) is also missing Address offset and System reset value.

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    June 19, 2018
    Posted on June 19, 2018 at 11:20

    Hello

    Bonnes.Uwe

    ,

    You are right, the description will be changed to:

    Bit 9 ADC2_DMA_RMP[1]: ADC2 DMA controller remapping bit

    0: Reserved

    1: ADC2 mapped on DMA1

    We will add the

    missing Address offset and System reset value:

    • Address offset:

      0x50

    • System reset value:

      0x200

    This is

    rasied internally for update in the coming release of the reference manual RM0

    With Regards,

    Imen.

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks