Skip to main content
Uwe Bonnes
Chief
September 21, 2017
Question

STM32H7 ADC speed

  • September 21, 2017
  • 7 replies
  • 2068 views
Posted on September 21, 2017 at 19:46

Hello,

the STM32H753bi.pdf datasheet Rev1 tells on page 2:

3× ADCs with 16-bit max. resolution (14 bits2.7 MSPS, 16 bits 168 kSPS)

This would imply a 14-bit SAR adc and 16 bit as a result of oversampling.

In chapter 6.3.20 16-bit ADC characteristics on page 157 of the dataheet however a sampling rate of 3.6 MSPS for 16-bit is given. This implies a 16-bit SAR block.

What holds?

    This topic has been closed for replies.

    7 replies

    Uwe Bonnes
    Chief
    September 28, 2017
    Posted on September 28, 2017 at 15:32

    Can somebody clarify?

    ST Technical Moderator
    September 28, 2017
    Posted on September 28, 2017 at 16:59

    Hello

    Bonnes.Uwe

    In fact, it is a

    16-bit SAR and w

    e are updating in the next datasheet version the first/

    preliminary

    data mentioned on page 2.

    Thanks and Kind Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Vladimir Vershinin
    Visitor II
    April 5, 2018
    Posted on April 05, 2018 at 11:41

    Hello,

    The STM32H743xI Reference manual (RM0433) section 25.3.13 'Channel-wise programmable sampling time (SMPR1, SMPR2) -> Constraints on the sampling time for fast and slow channels' says:

    For each channel, SMP[2:0] bits must be programmed to respect a minimum sampling time as specified in the ADC characteristics section of the datasheets.

    But the STM32H743xI datasheet Rev.3 section 6.3.20 '16-bit ADC characteristics' not contain the specification for slow channels.

    For example, the STM32L496xx datasheet the accuracy, sampling rate etc. is specified for both  ADC channels

    In addition, Table 78. 'ADC accuracy' (ENOB, SINAD, SNR, THD) not contain information about analog input frequency.

    Is it possible to obtain more detail data on the STH32H7 ADC performance?

    Thanks

    Singh.Harjit
    Senior
    April 29, 2018
    Posted on April 29, 2018 at 19:02

    Am assigning pins and would like to know the fast / slow ADC channel characteristics. Please provide info. or timeline. Thanks.

    Vladimir Vershinin
    Visitor II
    May 3, 2018
    Posted on May 03, 2018 at 09:33

    I applied to ST online technical support and their response was:

    ''In fact there is a typo in the datasheet. ''Fast'' should be replaced by ''Slow''

    in the last line in the table in the datasheet as shown by the attached image.  

    This will be corrected in the next version of the datasheet.''

    0690X0000060Ay5QAE.png
    Singh.Harjit
    Senior
    May 5, 2018
    Posted on May 05, 2018 at 18:44

    Thank you! Does anyone know the timeline for the next datasheet version?

    ST Technical Moderator
    June 7, 2018
    Posted on June 07, 2018 at 11:44

    Hello,

    We corrected this typo in the ''ADC characteristics'' table for the STM32H753xI datasheet Rev4 which is available since 18-May-2018.

    Thank you for bringing this issue to our attention.

    0690X0000060LBHQA2.png

    With Regards,

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks