Question
STM32F103C8 Peripheral Alternate Function
Posted on June 14, 2012 at 15:55
On the STM32F103C8 chip I can use the PA9 default alternate function to use either USART1_TX or TIM1_CH2 on that pin depending upon which peripheral is enabled.
If both peripherals are enabled and I am using PA9 as USART1_TX, does this preclude me from using TIM_CH1, TIM_CH3, or TIM_CH4?
This assumes that TIM_CH2 is disabled: TIM1 MOE =1 OSSR = x CC2E = 0 CC2NE = 0 I pretty sure the answer is ''Yes'', but would like confirmation. Thank you. #stm32