Skip to main content
np1
Associate III
April 10, 2015
Question

stop, standby mode with ADC

Posted on April 10, 2015 at 06:49

Hi all,

When I using ADC it work correctly, but when I want MCU enter STOP(or standby) mode and wakup by external interrupt, ADC is hang, can not convert ADC.

/**

  ******************************************************************************

  * @file    PWR_STOP/main.c 

  * @author  MCD Application Team

  * @version V1.1.0

  * @date    20-September-2012

  * @brief   Main program body

  ******************************************************************************

  * @attention

  *

  * <h2><center>&copy; COPYRIGHT 2012 STMicroelectronics</center></h2>

  *

  * Licensed under MCD-ST Liberty SW License Agreement V2, (the ''License'');

  * You may not use this file except in compliance with the License.

  * You may obtain a copy of the License at:

  *

  *        http://www.st.com/software_license_agreement_liberty_v2

  *

  * Unless required by applicable law or agreed to in writing, software 

  * distributed under the License is distributed on an ''AS IS'' BASIS, 

  * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.

  * See the License for the specific language governing permissions and

  * limitations under the License.

  *

  ******************************************************************************

  */ 

/* Includes ------------------------------------------------------------------*/

#include ''main.h''

/** @addtogroup STM32F3_Discovery_Peripheral_Examples

  * @{

  */

/** @addtogroup PWR_STOP

  * @{

  */ 

  #if 1

/* Private typedef -----------------------------------------------------------*/

/* Private define ------------------------------------------------------------*/

/* Private macro -------------------------------------------------------------*/

/* Private variables ---------------------------------------------------------*/

RTC_TimeTypeDef   RTC_TimeStructure;

RTC_InitTypeDef   RTC_InitStructure;

RTC_AlarmTypeDef  RTC_AlarmStructure;

EXTI_InitTypeDef EXTI_InitStructure;

NVIC_InitTypeDef NVIC_InitStructure;

__IO uint32_t TimingDelay;

/* Private function prototypes -----------------------------------------------*/

void Delay(__IO uint32_t nTime);

__IO uint16_t  ADC1ConvertedValue = 0, ADC1ConvertedVoltage = 0, calibration_value = 0;

__IO uint32_t TimingDelay = 0;

ADC_InitTypeDef       ADC_InitStructure;

ADC_CommonInitTypeDef ADC_CommonInitStructure;

GPIO_InitTypeDef      GPIO_InitStructure;

/* Private functions ---------------------------------------------------------*/

int main(void)

{

  /*!< At this stage the microcontroller clock setting is already configured, 

       this is done through SystemInit() function which is called from startup

       file (startup_stm32f30x.s) before to branch to application main.

       To reconfigure the default setting of SystemInit() function, refer to

       system_stm32f30x.c file

     */ 

  /* Configure the ADC clock */

  RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div2);

  

  /* Enable ADC1 clock */

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE);

      

  /* Setup SysTick Timer for 1 µsec interrupts  */

  if (SysTick_Config(SystemCoreClock / 1000000))

  { 

    /* Capture error */ 

    while (1)

    {}

  }

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);

   /* Configures the USER button */

  STM_EVAL_PBInit(BUTTON_USER,BUTTON_MODE_EXTI);

  /* ADC Channel configuration */

  /* GPIOC Periph clock enable */

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);

  /* Configure ADC Channel7 as analog input */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 ;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

  

  ADC_StructInit(&ADC_InitStructure);

  /* Calibration procedure */  

  ADC_VoltageRegulatorCmd(ADC1, ENABLE);

  

  /* Insert delay equal to 10 µs */

  Delay(10);

  

  ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single);

  ADC_StartCalibration(ADC1);

  

  while(ADC_GetCalibrationStatus(ADC1) != RESET );

  calibration_value = ADC_GetCalibrationValue(ADC1);

     

  ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;                                                                    

  ADC_CommonInitStructure.ADC_Clock = ADC_Clock_AsynClkMode;                    

  ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;             

  ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot;                  

  ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0;          

  ADC_CommonInit(ADC1, &ADC_CommonInitStructure);

  

  ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Enable;

  ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; 

  ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_0;         

  ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_None;

  ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

  ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable;   

  ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable;  

  ADC_InitStructure.ADC_NbrOfRegChannel = 1;

  ADC_Init(ADC1, &ADC_InitStructure);

  

  /* ADC1 regular channel7 configuration */ 

  ADC_RegularChannelConfig(ADC1, ADC_Channel_7, 1, ADC_SampleTime_7Cycles5);

  /* Enable ADC1 */

  ADC_Cmd(ADC1, ENABLE);

  /* wait for ADRDY */

  while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY));

  /* Start ADC1 Software Conversion */ 

  ADC_StartConversion(ADC1);   

      /* Request to enter STOP mode with regulator in low power mode */

   // PWR_EnterSTOPMode(PWR_Regulator_LowPower, PWR_STOPEntry_WFI);

  /* Infinite loop */

  while (1)

  {

    /* Test EOC flag */

    while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);

    

    /* Get ADC1 converted data */

    ADC1ConvertedValue =ADC_GetConversionValue(ADC1);

    

    /* Compute the voltage */

    ADC1ConvertedVoltage = (ADC1ConvertedValue *3300)/0xFFF;

    

  }

}

Please give me a help.

Thanks
    This topic has been closed for replies.

    1 reply

    np1
    np1Author
    Associate III
    April 10, 2015
    Posted on April 10, 2015 at 06:50

    I am using stm32f303