Skip to main content
dsystem
Associate II
May 21, 2018 2:58 PM UTC
Question

Motor Profiler fails

Posted on May 21, 2018 at 16:58

My end aim is to use #Motor #profiler to workout my motor parameters. I have #nucleo-F302R8 and #X-nucleo-IHM08M1 boards.

I selected these two in Profiler, Connected My motor and Hall devices, Entered 4 Pole pairs and max speed as 4000RPM. Max current as 20A (Motor rated for 30A). Connected Power suppy of 12V/40A . Connected and started Profiling.

Motor moved approx a revolution and stopped. And the after a few minutes and fails. Shows Resistance, Inductance, Supply voltage and current.

What is I am missing ??

Regards

Vimal Amin

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
Jun 28, 2021 4:57 AM UTC

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards